Performance SDMA transfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Performance SDMA transfer

ソリューションへジャンプ
1,963件の閲覧回数
larstraeger
Contributor II

Hello community,

i'd like to know which type of " uart 2 external memory" sdma transfer is faster. Should i use a shared Uart connect to SDMA via SPBA or is the access over the Functional Unit Peripheral/Burst Units for "normal" Uarts faster.

thanks and regards

Lars

ラベル(3)
0 件の賞賛
返信
1 解決策
1,622件の閲覧回数
JerryFan
NXP Employee
NXP Employee

SPBA bus is preferred, since it is dedicated to SDMA, and thus bus swithch, bus competition(specailly for IP bus which connected with a lot of peripheral), if Functional Unit Peripheral used,  can be avoided.  

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,623件の閲覧回数
JerryFan
NXP Employee
NXP Employee

SPBA bus is preferred, since it is dedicated to SDMA, and thus bus swithch, bus competition(specailly for IP bus which connected with a lot of peripheral), if Functional Unit Peripheral used,  can be avoided.  

0 件の賞賛
返信