i.MX233 and SDIO multiplex

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX233 and SDIO multiplex

Jump to solution
2,466 Views
daveshah
Contributor I

Would it be possible to have both an SDIO wireless device and an SDHC card on one SSP of the i.MX233, using a multiplexer like TS3A27518E-Q1 or MAX4996? Also, could you do it simply by connecting the data lines together for the two cards and having separate CMD lines for each device?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,040 Views
JackyAtFreescal
Senior Contributor II

Quote from "SD Specifications Part 1 Physical Layer Specification Version 2.00"

3.5 Bus Topology

...

Common bus signals for multiple card slots are not recommended. A single SD bus should

connect a single SD card.

...

Regards,

Jacky

View solution in original post

0 Kudos
Reply
2 Replies
2,040 Views
YixingKong
Senior Contributor IV

Hi David, did Jacky's answer helps you. If yes, please mark it as Correct Answer.

0 Kudos
Reply
2,041 Views
JackyAtFreescal
Senior Contributor II

Quote from "SD Specifications Part 1 Physical Layer Specification Version 2.00"

3.5 Bus Topology

...

Common bus signals for multiple card slots are not recommended. A single SD bus should

connect a single SD card.

...

Regards,

Jacky

0 Kudos
Reply