i.MX 8MM secure boot: The difference between "CONFIG_SECURE_BOOT" and "CONFIG_IMX_HAB"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX 8MM secure boot: The difference between "CONFIG_SECURE_BOOT" and "CONFIG_IMX_HAB"

跳至解决方案
1,798 次查看
callme_friend
Contributor I

I tried the Secure Boot of I.MX 8mm. When looking at the information, I saw "config_secure_boot" and "config_imx_hab", and there were Guide documents under U-Boot/DOC: doc/imx/ahab/  doc/imx/habv4/

 

What is the difference between HABv4 and aHAB?

Is there a more detailed explanation document?

0 项奖励
回复
1 解答
1,778 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @callme_friend,

I hope you are doing well.

CONFIG_SECURE_BOOT option is replaced with CONFIG_IMX_HAB in the newer BSP using the below commit.

 
HABv4 and AHAB are both different secure-boot concept.
 
AHAB is new secure-boot concept used in i.MX 8/8x/8ULP/9x family of applications processors
&
HABv4 is available in i.MX 50, i.MX 53, i.MX 6, i.MX 7 series and i.MX 8M family of applications processors
 
Please refer to the documents.

在原帖中查看解决方案

1 回复
1,779 次查看
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @callme_friend,

I hope you are doing well.

CONFIG_SECURE_BOOT option is replaced with CONFIG_IMX_HAB in the newer BSP using the below commit.

 
HABv4 and AHAB are both different secure-boot concept.
 
AHAB is new secure-boot concept used in i.MX 8/8x/8ULP/9x family of applications processors
&
HABv4 is available in i.MX 50, i.MX 53, i.MX 6, i.MX 7 series and i.MX 8M family of applications processors
 
Please refer to the documents.