i.MX 8M Nano secondary boot image on spi boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

i.MX 8M Nano secondary boot image on spi boot

跳至解决方案
1,926 次查看
lelle
Contributor I

Hello,

 

We’re planning implementation of having a fail-safe update mechanism for bootloader (u-boot) and would like to utilize the “Secondary image boot” feature. Our board boots from 4MB serial NOR over SPI (ECSPI1).

Bootloader is typically divided into two parts, SPL (loaded by CPU) and u-boot (loaded by SPL). The both parts are likely to be dependent on specific configuration of each other and should be updated as a pair.

This is difficult to achieve without knowing if we have booted using “Primary Image boot” or “secondary Image boot”.

Boot flow diagram of reference manual mentions an image index persistent bit.

Does the CPU BOOT ROM store this information in any register or is it possible to somehow find out?

lelle_0-1680597899291.png


Regards,

Lelle

标签 (1)
0 项奖励
回复
1 解答
1,904 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport
Hi @lelle ,
 
I hope you are doing well.
 
Information about persistent bits is removed and additional info is not made public in the latest version of RM as it is not required by users.
 
ROM sets PERSIST_SECONDARY_BOOT (SRC_GPR10[30]) bit to 1 if the primary boot image is corrupted or bad
 
It is required to fuse IMG_CNTN_SET1_OFFSET to support the secondary boot in i.MX8MN.
 
Please refer to 6.1.6.2 Secondary Image Boot in i.MX 8M Nano Applications Processor Reference Manual.
 
Thanks & Regards,
Sanket Parekh

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,905 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport
Hi @lelle ,
 
I hope you are doing well.
 
Information about persistent bits is removed and additional info is not made public in the latest version of RM as it is not required by users.
 
ROM sets PERSIST_SECONDARY_BOOT (SRC_GPR10[30]) bit to 1 if the primary boot image is corrupted or bad
 
It is required to fuse IMG_CNTN_SET1_OFFSET to support the secondary boot in i.MX8MN.
 
Please refer to 6.1.6.2 Secondary Image Boot in i.MX 8M Nano Applications Processor Reference Manual.
 
Thanks & Regards,
Sanket Parekh
0 项奖励
回复
820 次查看
junya
Contributor IV

Hi @Sanket_Parekh ,

I have two questions.
∙ Is the PERSIST_SECONDARY_BOOT information also removed from the latest RM for i.mx8mp?

∙ If the boot device is a nandflash, does the primary boot fail if the u-boot area is not linear due to the presence of bad blocks?

 

Best regards,

sakemi

0 项奖励
回复
1,861 次查看
lelle
Contributor I

Hello,

Thank you, this is precisely what I'm looking for.

Regards,

lelle

0 项奖励
回复