i.MX 8M NANO EVK with display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 8M NANO EVK with display

2,583 次查看
Rohan_R_E
Contributor II

I am using i.MX 8M NANO Evaluation kit connected with 10.5inch Capacitive Touch AMOLED, HDMI, 2560×1600 2K Resolution, Optical Bonding. I can find that "fsl-imx8mn-ddr4-evk-rm67191.dtb" fdt file is booting up but getting error at the last as mentioned below and supports only one resolution 1080x1920.
Please do guide me to resolve the errors and also provide an fdt file that supports 2560x1600 2k resolution.
imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[ 7.571675] panel-raydium-rm67191 32e10000.mipi_dsi.0: [drm:rad_panel_enable] *ERROR* Failed to send MCS (-16)
[ 7.581734] imx_sec_dsim_drv 32e10000.mipi_dsi: panel enable failed: -16

iMX8MNANO 

 

标签 (1)
0 项奖励
回复
3 回复数

2,553 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can refer to the driver for rm76191, change it according to your panel

https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/drivers/gpu/drm/panel/panel-raydium-rm67191.c

static const struct drm_display_mode default_mode = {
.clock = 121000,
.hdisplay = 1080,
.hsync_start = 1080 + 20,
.hsync_end = 1080 + 20 + 2,
.htotal = 1080 + 20 + 2 + 34,
.vdisplay = 1920,
.vsync_start = 1920 + 10,
.vsync_end = 1920 + 10 + 2,
.vtotal = 1920 + 10 + 2 + 4,
.width_mm = 68,
.height_mm = 121,
.flags = DRM_MODE_FLAG_NHSYNC |
DRM_MODE_FLAG_NVSYNC,
};

2,533 次查看
Rohan_R_E
Contributor II

Hi Joanxie,

Thank you for your response. I would like to get the detailed instructions for making the changes in the drm rm76191 including the path of the file and how to compile the file and boot on the i.MX 8M nano Evk board. It will be of great help for me.

Thank you,

Rohan R E

0 项奖励
回复

2,503 次查看
joanxie
NXP TechSupport
NXP TechSupport

don't have such document, you need porting by yourself according to rm67191, if you have any issue when you porting, you can contact us, for how to deploy and build uboot or kernel, you can refer to the enclosed file

if you need nxp help you porting, you can consult this from professional support

"https://www.nxp.com/support/support/nxp-engineering-services/professional-support-for-processors-and..."

0 项奖励
回复