i.MX 6Solox M4 programming using Uboot for udoo board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX 6Solox M4 programming using Uboot for udoo board

1,209 次查看
armk
Contributor I

Hi,

I am using i.MX 6solox on udoo board. On A9 i have linux running successfully. I want to program the M4 using u boot , there is no QSPI on the board. I am noob in Linux. I understand that the U-boot is made custom to hardware layout. In this case I wont be able to use the U-boot provided by the freescale?. Can anyone help me to start this?

Thank You

标签 (3)
0 项奖励
回复
1 回复

945 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the following :

“Loading Code on Cortex-M4 from Linux for the i.MX 6SoloX and i.MX 7Dual/7Solo Application Processors”

 

http://www.nxp.com/assets/documents/data/en/application-notes/AN5317.pdf 

MX6 SoloX bare metal startup  

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 项奖励
回复