i.MX 6Solox M4 programming using Uboot for udoo board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX 6Solox M4 programming using Uboot for udoo board

1,207件の閲覧回数
armk
Contributor I

Hi,

I am using i.MX 6solox on udoo board. On A9 i have linux running successfully. I want to program the M4 using u boot , there is no QSPI on the board. I am noob in Linux. I understand that the U-boot is made custom to hardware layout. In this case I wont be able to use the U-boot provided by the freescale?. Can anyone help me to start this?

Thank You

ラベル(3)
0 件の賞賛
返信
1 返信

943件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the following :

“Loading Code on Cortex-M4 from Linux for the i.MX 6SoloX and i.MX 7Dual/7Solo Application Processors”

 

http://www.nxp.com/assets/documents/data/en/application-notes/AN5317.pdf 

MX6 SoloX bare metal startup  

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信