hwclock --systohc not Working on imx6sl

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hwclock --systohc not Working on imx6sl

2,038 Views
sandeepajesh
Contributor III

Dear NXP Experts,

I am working on  imx6sl board and I am not able to sync hardware clock with system time.

When I execute hwclock --systohc system gets hanged.

Please help.

Regards

Sandeep S

Labels (1)
0 Kudos
Reply
2 Replies

1,614 Views
b36401
NXP Employee
NXP Employee

Please try to play with start/stop /etc/init.d/hwclock.sh service.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,614 Views
sandeepajesh
Contributor III

HI

Issue was with SoC revision. After upgrading to Soc version 1.2 hwclock is working fine.

0 Kudos
Reply