hwclock --systohc not Working on imx6sl

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hwclock --systohc not Working on imx6sl

1,938 次查看
sandeepajesh
Contributor III

Dear NXP Experts,

I am working on  imx6sl board and I am not able to sync hardware clock with system time.

When I execute hwclock --systohc system gets hanged.

Please help.

Regards

Sandeep S

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,514 次查看
b36401
NXP Employee
NXP Employee

Please try to play with start/stop /etc/init.d/hwclock.sh service.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,514 次查看
sandeepajesh
Contributor III

HI

Issue was with SoC revision. After upgrading to Soc version 1.2 hwclock is working fine.

0 项奖励
回复