how to make secure boot of kernel and RFS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to make secure boot of kernel and RFS

ソリューションへジャンプ
1,978件の閲覧回数
PramodKumar
Contributor IV

Hi,

Please help us to make encrypted kernel and RFS and boot the i.MX233 based board.

Regards,

Pramod Kumar

タグ(6)
0 件の賞賛
返信
1 解決策
1,702件の閲覧回数
Yuri
NXP Employee
NXP Employee

   The i.MX23 supports encrypted boot, described in section  5.1 (i.MX28 encrypted boot in a nut-shell)
of the app note AN4555 (Secure Boot with i.MX28 HAB Version 4). Also please refer to Chapter 35

(Boot Modes) of the i.MX23 Reference Manual. Note, the i.MX23 does not support HAB technology.

  So, it is possible to use encrypted boot of a bootloader ( say, U-boot) and further activities regarding
kernel and RFS should be performed by U-boot. Sorry, we do not have an app note about this.

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,703件の閲覧回数
Yuri
NXP Employee
NXP Employee

   The i.MX23 supports encrypted boot, described in section  5.1 (i.MX28 encrypted boot in a nut-shell)
of the app note AN4555 (Secure Boot with i.MX28 HAB Version 4). Also please refer to Chapter 35

(Boot Modes) of the i.MX23 Reference Manual. Note, the i.MX23 does not support HAB technology.

  So, it is possible to use encrypted boot of a bootloader ( say, U-boot) and further activities regarding
kernel and RFS should be performed by U-boot. Sorry, we do not have an app note about this.

Regards,

Yuri.

0 件の賞賛
返信