how to change partition of imx8qm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to change partition of imx8qm

1,343 Views
XiaofengZang
Contributor III

Hello

i'm debugging imx8qm evm, how to modify emmc partition of this board?

i modify mksdcard-android.sh.tar of mfgtool, partition is not changed.

Thanks

Tags (1)
0 Kudos
Reply
2 Replies

1,209 Views
b36401
NXP Employee
NXP Employee

Please note that accordingly to eMMC specifications boot partition size is fixed during production.
Its size is defined in EXT_CSD structure of the eMMC.
It is not recommended to change boot partition size.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,209 Views
XiaofengZang
Contributor III

we use android o system

0 Kudos
Reply