how to change partition of imx8qm

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to change partition of imx8qm

1,341件の閲覧回数
XiaofengZang
Contributor III

Hello

i'm debugging imx8qm evm, how to modify emmc partition of this board?

i modify mksdcard-android.sh.tar of mfgtool, partition is not changed.

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,207件の閲覧回数
b36401
NXP Employee
NXP Employee

Please note that accordingly to eMMC specifications boot partition size is fixed during production.
Its size is defined in EXT_CSD structure of the eMMC.
It is not recommended to change boot partition size.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,207件の閲覧回数
XiaofengZang
Contributor III

we use android o system

0 件の賞賛
返信