how to calculate the time in table 44-8. MMDC Refresh Scheme

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to calculate the time in table 44-8. MMDC Refresh Scheme

2,377 Views
masatsuguyamada
Contributor II

Hi,
I have a question about i.MX6 document,
http://www.nxp.com/assets/documents/data/en/reference-manuals/IMX6DQRM.pdf
p.3848, Table 44-8. MMDC Refresh Scheme.

The column "Description" of the table describes,

Option numberDescriptionREF_SEL
131,250 ns64 KHz
215,625 ns32 KHz

I understood the interval time in "Description" is related to REF_SEL, but I couldn't understand how to calculate.

My question is how to calculate the interval time described in "Description".
It seems the time is not inverse number of the frequency(REF_SEL).

However this interval time seems right from my experiment using DDR Stress Test.
I tried two test case (REFR is same value for purpose),
(1) REFR=0x3 REF_SEL=0 (64KHz)
(2) REFR=0x3 REF_SEL=1 (32KHz)
and (1) was failed within 400~500 loops, (2) was continued over 1000 loops.

Thanks in advance,
Yamada

Labels (1)
4 Replies

2,103 Views
Yuri
NXP Employee
NXP Employee

Hello

   I think it would be better to look at tables in section 44.12.9 [MMDC Core Refresh

Control Register (MMDCx_MDREF)] of the RM.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply

2,103 Views
masatsuguyamada
Contributor II

Thanks for advice! actually, I tried the Stress Test with REF_SEL=32/64KHz, and
when I changed REF_SEL to 64KHz from 32KHz, the system became easier to fail.

Also before my trial, I thought the refresh rate of
(a) REF_SEL=32KHz REFR=0x7 (8 Refreshes)
(b) REF_SEL=64KHz REFR=0x3 (4 Refreshes)
will be same, but in the Stress Test, (a) was stable, but (b) was failed at early loop (100~200 loops).

So I wish to know how REF_SEL affect to refresh rate. I thought if Description column in the Table 44-8 is true, above result can be explained.

Regards,
Yamada

0 Kudos
Reply

2,103 Views
Yuri
NXP Employee
NXP Employee

Hello,

   

  Your understanding of how the refresh rate should be calculated is correct,

assuming that DRAM part should be fully refreshed within a specified Refresh

Window (usually 64 ms, but LPDDR2 has temperature dependence here, may

be 32 ms).

 

  Configurations

 

(a) REF_SEL=32KHz with REFR=0x7 (8 Refreshes)

and

(b) REF_SEL=64KHz (both edges of 32KHz is involved) with REFR=0x3 (4 Refreshes)

 

are the same. NXP recommends 32KHz variant using.

 

  “The way that parameter tREFI is determined (for LPDDR2) is to count up all the refreshes within

a specified Refresh Window (32 ms for T<85C), and then divide 32 ms by the number received to get

the average tREFI.”

 

  Is Your DRAM - LPDDR2 ?

Please double check design using the following design checklist

 

https://community.nxp.com/docs/DOC-93819 

Regards,

Yuri.

0 Kudos
Reply

2,103 Views
masatsuguyamada
Contributor II

Thank you very much! My question about REF_SEL / REFR  was resolved.

The HW structure is following ( using DDR3 ).
- i.MX6  ( MCIMX6Q7CVT08AC )
- DDR3 DRAM ( mt41k256m16ha,  https://www.micron.com/parts/dram/ddr3-sdram/mt41k256m16ha-125-it )

Excel file in the linked site will be helpful, I will check it with HW team.

Regards,
Yamada