Hi Can i use VM option on my windows machine for iMX8 QuadMax MEK development?
If yes what is the required configuration for the host machine?
Also please give some details about the VM configuration as well.
Hi @Frantisek_Prochaska @brian14 ,
Sorry for the delay in reply.
I want to use build the software related to iMX8QuadMax MEK board on my Windows laptop which has Ubuntu 22.04 running on the VirutalBox.
I want to know weather there is any specific system configuartion required for this like how much RAM, FLASH be assigned to the Ubuntu running on the VirtualBox or is a seperate Laptop/workstation with Ubuntu required to do any developmnt work related to the iMX8QuadMax board?
Also let me know if there is any specific workstation hardware requirements needed to work with this board?
Hi @mshanka1,
Thank you for your reply.
Based on The Yocto Project User's Guide:
"The minimum hard disk space required is about 50 GB. It is recommended that at least 120 GB is provided, which is enough to compile all backends together. For building machine learning components, at least 250 GB is recommended. The recommended minimum Ubuntu version is 20.04 or later. The latest release supports Chromium v91, which requires an increase to the ulimit (number of open files) to 4098."
Regarding RAM space, in my experience I would say that you will need a minimum of 8 GB to have correct operation.
I hope this information will be helpful.
Have a great day!
Hi @brian14 ,
Thank for the information.
My laptop configuration is:
Windows 10 Pro,
RAM: 16GB
Memory: 500GB.
I have installed VistualBox and installed Ubuntu 22.04 over virtual box.
I have selected RAM: 4GB, Disk Space: 25GB.
Should i have to select RAM: 8GB and Disk Space: 120GB for iMX8QuadMax MEK to work properly (BSP compilation etc). I am not going for any Machine Language development projects.
 Frantisek_Proch
		
			Frantisek_Proch