gstreamer1.0-plugins-imx build fail on IMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

gstreamer1.0-plugins-imx build fail on IMX8MP

Jump to solution
1,113 Views
shlomz
Contributor III

HI,

when building gstreamer1.0-plugins-imx with yocto (6.1-langdale) it sequently builds libimxvpuapi2 which fails during its configuration stage on:

Checking for library hantro_h1 :
not found

The configuration failed

would appreciate the help.

 

thanks.

Tags (3)
0 Kudos
Reply
1 Solution
1,092 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Please share more details with what steps you've taken and error log. 

Like what DISTRO AND MACHINE you build with? 

I've tried to build with fsl-imx-wayland and imx8mp-lpddr4-evk. Found that some of open sources for this release have been changed. The BSP has been released a bit long. So, can you please use the new BSP and then built it? 

 

Regards

Harvey

View solution in original post

0 Kudos
Reply
5 Replies
1,093 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Please share more details with what steps you've taken and error log. 

Like what DISTRO AND MACHINE you build with? 

I've tried to build with fsl-imx-wayland and imx8mp-lpddr4-evk. Found that some of open sources for this release have been changed. The BSP has been released a bit long. So, can you please use the new BSP and then built it? 

 

Regards

Harvey

0 Kudos
Reply
1,088 Views
shlomz
Contributor III

im using a custom MACHINE which is basically aligned with imx8mp-lpddr-evk. 

I will try the new BSP and see if it works on imx8mp-lpddr-evk.

as I understand it, gstreamer1.0-plugins-imx should enable freerdp to work with the gstremer libs and thus have hw acceleration on vpu enabled, is it correct?

0 Kudos
Reply
1,068 Views
Harvey021
NXP TechSupport
NXP TechSupport

Is the build working for you with new BSP? 

About the freerdp to work with gstremer libs, please raise a new ticket for further assistance.

 

Regards

Harvey

 

0 Kudos
Reply
1,065 Views
shlomz
Contributor III

yes, but only after updating the src for libimxvpuapi2 to a commit that includes this fix:

https://github.com/Freescale/libimxvpuapi/pull/62/commits/7ad208c83515c34f54200614e3ac6940a9dfb0fa

Otherwise, I get the same linker error during the build.

I suggest NXP updates the recipe

 

thanks!

0 Kudos
Reply
1,062 Views
Harvey021
NXP TechSupport
NXP TechSupport

Thank you, already inform the same to internal team for these updates.

 

Regards

Harvey

0 Kudos
Reply