gstream to images

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,160件の閲覧回数
yennivenkateswa
Contributor II

hi,

i am using imx53 board with additional csi interface hardware. i am getting stream using ./mxc_v4l2_tvin.out -ow 480 -oh 480.

now i want images from this streaming and i want to record video using this stream. i dont know how to record or capture images.

can anyone help to solve this prloblem and refer any materials.

Thanks&Regards

venkatesh

ラベル(6)
0 件の賞賛
返信
1 解決策
1,732件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,733件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
1,733件の閲覧回数
Yuri
NXP Employee
NXP Employee

   In order to record a video from a cam one can use the gstreamer, as an example  :

$gst-launch mfw_v4lsrc fps-n=15 capture-width=$WIDTH capture-height=$HEIGHT ! queue ! mfw_vpuencoder codec-type=0 ! avimux ! filesink location=output.avi sync=false

Please refer to "Linux_Multimedia_Framework_User_Guide.pdf" in codec package.

https://www.freescale.com/webapp/Download?colCode=IMX53_11_09_LINUX_MMCODECS&appType=license&locatio...

Summary Page :

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&fpsp=1&tab=Design_Tools_Tab

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信