git clone kernel_imx fail ???

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

git clone kernel_imx fail ???

2,677 次查看
glj
Contributor I

lmd@ubuntu:~/android442$ git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx
Cloning into 'kernel_imx'...
fatal: read error: Connection reset by peer

标签 (1)
0 项奖励
回复
3 回复数

2,344 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi all,

Please note that for one or the other reason the GIT server is sometimes not reachable, but you still have the option to download the source code from Freescale Public GIT  (http://git.freescale.com/git/) and then build it. If you have the need for various builds based on the same release, then it's useful to download all sources one time and base the following builds then on (a copy of) the local sources:


$ bitbake -c fetchall target


In Yocto Project Development Manual (http://www.yoctoproject.org/docs/2.0/dev-manual/dev-manual.html) in chapter 5.15 you find some more information.

On the other hand, verify that you have internet connection and you may contact your system administrator because if you are using firewalls or porxy server this may avoid conenction.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,344 次查看
jesse_zbikowski
Contributor I

Glad to hear it's working for you - I saw a similar error and was able to make progress by cloning only the single branch I needed:

git clone -b imx_4.9.11_1.0.0_ga  --single-branch git://git.freescale.com/imx/linux-imx.git

0 项奖励
回复

2,344 次查看
glj
Contributor I

Now it is ok! 

0 项奖励
回复