gdb setup for imx287 evk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

gdb setup for imx287 evk

1,591 次查看
ask
Contributor III

I am trying to setup the gdb setup for imx287 evk board as per the attached document.  gdb version I used is 7.4.

I struck at step no 6 in the section 4, i.e not able to build native version(including gdb server).

Please can any one help out by providing the commands for the step no 6. In the document it has been given for imx6.

0 项奖励
回复
1 回复

1,427 次查看
igorpadykov
NXP Employee
NXP Employee

Hi ashok

I think you can try below steps for i.MX23

Debugging the iMX233-OLinuXino via SJTAG with OpenOCD — Christian's Blog

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复