fsl-community-bsp (Yocto dylan) on i.MX6 SABRE for Smart Devices: 10" display not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

fsl-community-bsp (Yocto dylan) on i.MX6 SABRE for Smart Devices: 10" display not working

跳至解决方案
6,739 次查看
c_hahn
Contributor III

Hi,

I am new to the i.MX6 community and trying to get Linux working on my new i.MX6 Series SABRE for Smart Devices board (MCIMX6Q-SDP).

I got the repo tool and initiated a repo with

repo init -u https://github.com/Freescale/fsl-community-bsp-platform -b dylan

repo sync

Then I built a core-image-x11 with

source setup-environment build

bitbake core-image-x11

The build completed with

Build Configuration:

BB_VERSION        = "1.18.0"

BUILD_SYS         = "i686-linux"

NATIVELSBSTRING   = "SUSE-LINUX-11.4"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "poky"

DISTRO_VERSION    = "1.4"

TUNE_FEATURES     = "armv7a vfp neon"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):c3cb65041834159a318df9c1a5a05f1ef36a2ebc"

meta-oe           = "(nobranch):f3e293c3c81be161234fdc5d5e3329db24d3f30f"

meta-fsl-arm      = "(nobranch):95e013e931e64c4e2c09cce8b946e876baefac78"

meta-fsl-arm-extra = "(nobranch):5f5a9cfcad223f5a1c623346780510ffcdc012ab"

meta-fsl-demos    = "(nobranch):724cfb929748f47782dea3b1dc412b028f6f3515"

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

NOTE: multiple providers are available for jpeg-native (jpeg-native, libjpeg-turbo-native)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg-native

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

WARNING: Failed to fetch URL http://www.apache.org/dist/subversion/subversion-1.7.8.tar.bz2, attempting MIRRORS if available

WARNING: Failed to fetch URL http://downloads.sourceforge.net/project/libpng/libpng16/1.6.0/libpng-1.6.0.tar.xz, attempting MIRRORS if available

NOTE: Tasks Summary: Attempted 4675 tasks of which 508 didn't need to be rerun and all succeeded.

Summary: There were 2 WARNING messages shown.

Then I copied the ./build/tmp/deploy/images/core-image-x11-imx6qsabresd.sdcard file to an SD card with

dd if=core-image-x11-imx6qsabresd.sdcard of=/dev/sdd bs=1M

while /dev/sdd is the drive where my SD-card shows up in fdisk -l

I inserted the SD card into the board booted, but no penguins on the screen and no Yocto boot animation.

The display works with the Android SD card as well as when I am exchanging my self-made Kernel with the kernel that comes with the new

L3.0.35_4.0.0_DEMO_IMAGE that I found on SABRE Platform for Smart Devices Based on the i.MX 6 Series Product Summary Page

So I think the issue is a Kernel issue. (by the way, the Kernel from L3.0.35_4.0.0_DEMO_IMAGE does not work with the x-server from Yocto-dylan)

This is what I see as boot log on the serial console


U-Boot 2013.04-00038-ge035df3 (May 17 2013 - 10:01:39)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

Reset cause: POR

Board: MX6Q-SabreSD

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Warning: FEC using MAC address from net device

Hit any key to stop autoboot:  0

mmc1 is current device

reading boot.scr

** Unable to read file boot.scr **

reading uImage

3840468 bytes read in 182 ms (20.1 MiB/s)

Booting from mmc ...

reading imx6q-sabresd.dtb

** Unable to read file imx6q-sabresd.dtb **

## Booting kernel from Legacy Image at 12000000 ...

   Image Name:   Linux-3.0.35-12.09.01+yocto+g059

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    3840404 Bytes = 3.7 MiB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

   Loading Kernel Image ... OK

OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.

Linux version 3.0.35-12.09.01+yocto+g0596856 (acka@msc-ubuntu-acka) (gcc version 4.7.2 (GCC) ) #1 SMP PREEMPT Mon Apr 15 16:04:47 CEST 2013

CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d

CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine: Freescale i.MX 6Quad/DualLite/Solo Sabre-SD Board

Memory policy: ECC disabled, Data cache writealloc

CPU identified as i.MX6Q, silicon rev 1.2

PERCPU: Embedded 7 pages/cpu @8c008000 s5440 r8192 d15040 u32768

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 227328

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw

PID hash table entries: 4096 (order: 2, 16384 bytes)

Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)

Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)

Memory: 640MB 256MB = 896MB total

Memory: 896884k/896884k available, 151692k reserved, 0K highmem

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)

    DMA     : 0xf4600000 - 0xffe00000   ( 184 MB)

    vmalloc : 0xc0800000 - 0xf2000000   ( 792 MB)

    lowmem  : 0x80000000 - 0xc0000000   (1024 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .init : 0x80008000 - 0x8003b000   ( 204 kB)

      .text : 0x8003b000 - 0x80a86b4c   (10543 kB)

      .data : 0x80a88000 - 0x80ae8220   ( 385 kB)

       .bss : 0x80ae8244 - 0x80b350f0   ( 308 kB)

SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=4, Nodes=1

Preemptible hierarchical RCU implementation.

NR_IRQS:496

MXC GPIO hardware

sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 1431655ms

MXC_Early serial console at MMIO 0x2020000 (options '115200')

bootconsole [ttymxc0] enabled

Console: colour dummy device 80x30

Calibrating delay loop... 1581.05 BogoMIPS (lpj=7905280)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 512

CPU: Testing write buffer coherency: ok

hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available

CPU1: Booted secondary processor

CPU2: Booted secondary processor

CPU3: Booted secondary processor

Brought up 4 CPUs

SMP: Total of 4 processors activated (6324.22 BogoMIPS).

devtmpfs: initialized

print_constraints: dummy:

NET: Registered protocol family 16

print_constraints: vddpu: 725 <--> 1300 mV at 1100 mV fast normal

print_constraints: vddcore: 725 <--> 1300 mV at 1100 mV fast normal

print_constraints: vddsoc: 725 <--> 1300 mV at 1200 mV fast normal

print_constraints: vdd2p5: 2000 <--> 2775 mV at 2400 mV fast normal

print_constraints: vdd1p1: 800 <--> 1400 mV at 1100 mV fast normal

print_constraints: vdd3p0: 2800 <--> 3150 mV at 3000 mV fast normal

hw-breakpoint: found 6 breakpoint and 1 watchpoint registers.

hw-breakpoint: 1 breakpoint(s) reserved for watchpoint single-step.

hw-breakpoint: maximum watchpoint size is 4 bytes.

L310 cache controller enabled

l2x0: 16 ways, CACHE_ID 0x410000c7, AUX_CTRL 0x02070000, Cache size: 1048576 B

IMX usb wakeup probe

bio: create slab <bio-0> at 0

print_constraints: SPKVDD: 4200 mV

print_constraints: vmmc: 3300 mV

SCSI subsystem initialized

spi_imx imx6q-ecspi.0: probed

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

Freescale USB OTG Driver loaded, $Revision: 1.55 $

add wake up source irq 75

mc_pfuze 1-0008: ID: 0,Full lay: 1 ,Metal lay: 1

mc_pfuze 1-0008: FAB: 0 ,FIN: 0

print_constraints: PFUZE100_SW1A: 300 <--> 1875 mV at 1375 mV

print_constraints: PFUZE100_SW1B: 300 <--> 1875 mV at 300 mV

print_constraints: PFUZE100_SW1C: 300 <--> 1875 mV at 1375 mV

print_constraints: PFUZE100_SW2: 800 <--> 3950 mV at 3300 mV

print_constraints: PFUZE100_SW3A: 400 <--> 1975 mV at 1500 mV

print_constraints: PFUZE100_SW3B: 400 <--> 1975 mV at 1500 mV

print_constraints: PFUZE100_SW4: 800 <--> 3950 mV at 3150 mV

print_constraints: PFUZE100_SWBST: 5000 <--> 5150 mV at 5000 mV

print_constraints: PFUZE100_VSNVS: 1200 <--> 3000 mV at 1800 mV

print_constraints: PFUZE100_VREFDDR: at 750 mV

print_constraints: PFUZE100_VGEN1: 800 <--> 1550 mV at 1500 mV

print_constraints: PFUZE100_VGEN2: 800 <--> 1550 mV at 1500 mV

print_constraints: PFUZE100_VGEN3: 1800 <--> 3300 mV at 2500 mV

print_constraints: PFUZE100_VGEN4: 1800 <--> 3300 mV at 1800 mV

print_constraints: PFUZE100_VGEN5: 1800 <--> 3300 mV at 2800 mV

print_constraints: PFUZE100_VGEN6: 1800 <--> 3300 mV at 3300 mV

imx-ipuv3 imx-ipuv3.0: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

imx-ipuv3 imx-ipuv3.1: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 driver probed

mxc_mipi_csi2 mxc_mipi_csi2: i.MX MIPI CSI2 dphy version is 0x3130302a

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Version 1.0.24.

Bluetooth: Core ver 2.16

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

cfg80211: Calling CRDA to update world regulatory domain

max17135 2-0048: PMIC MAX17135 for eInk display

i2c-core: driver [max17135] using legacy suspend method

i2c-core: driver [max17135] using legacy resume method

Switching to clocksource mxc_timer1

NET: Registered protocol family 2

IP route cache hash table entries: 32768 (order: 5, 131072 bytes)

TCP established hash table entries: 131072 (order: 8, 1048576 bytes)

TCP bind hash table entries: 65536 (order: 7, 786432 bytes)

TCP: Hash tables configured (established 131072 bind 65536)

TCP reno registered

UDP hash table entries: 512 (order: 2, 16384 bytes)

UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

PMU: registered new PMU device of type 0

Static Power Management for Freescale i.MX6

wait mode is enabled for i.MX6

cpaddr = c0880000 suspend_iram_base=c08fc000

PM driver module loaded

IMX usb wakeup probe

i.MXC CPU frequency driver

JFFS2 version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

msgmni has been set to 1751

alg: No test for stdrng (krng)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

mxc_mipi_dsi mxc_mipi_dsi: i.MX MIPI DSI driver probed

MIPI DSI driver module loaded

mxc_sdc_fb mxc_sdc_fb.0: register mxc display driver ldb

_regulator_get: get() with no identifier

imx-ipuv3 imx-ipuv3.1: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)

Console: switching to colour frame buffer device 128x48

mxc_sdc_fb mxc_sdc_fb.1: register mxc display driver ldb

mxc_sdc_fb mxc_sdc_fb.2: register mxc display driver lcd

mxc_sdc_fb mxc_sdc_fb.3: register mxc display driver ldb

mxc_sdc_fb mxc_sdc_fb.3: ipu1-di1 already in use

mxc_sdc_fb: probe of mxc_sdc_fb.3 failed with error -16

mxc_sdc_fb mxc_sdc_fb.4: register mxc display driver ldb

mxc_sdc_fb mxc_sdc_fb.4: ipu1-di1 already in use

mxc_sdc_fb: probe of mxc_sdc_fb.4 failed with error -16

imx-sdma imx-sdma: loaded firmware 1.1

imx-sdma imx-sdma: initialized

Serial: IMX driver

imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX

console [ttymxc0] enabled, bootconsole disabled

console [ttymxc0] enabled, bootconsole disabled

loop: module loaded

Can't recover from RESET HBA!

No sata disk.

m25p80 spi0.0: found m25p32, expected sst25vf016b

m25p80 spi0.0: m25p32 (4096 Kbytes)

Creating 2 MTD partitions on "m25p80":

0x000000000000-0x000000100000 : "bootloader"

0x000000100000-0x000000400000 : "kernel"

vcan: Virtual CAN interface driver

CAN device driver interface

flexcan netdevice driver

FEC Ethernet Driver

fec_enet_mii_bus: probed

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1

fsl-ehci fsl-ehci.0: irq 75, io base 0x02184000

fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00

hub 1-0:1.0: USB hub found

hub 1-0:1.0: 1 port detected

add wake up source irq 72

fsl-ehci fsl-ehci.1: Freescale On-Chip EHCI Host Controller

fsl-ehci fsl-ehci.1: new USB bus registered, assigned bus number 2

fsl-ehci fsl-ehci.1: irq 72, io base 0x02184200

fsl-ehci fsl-ehci.1: USB 2.0 started, EHCI 1.00

hub 2-0:1.0: USB hub found

hub 2-0:1.0: 1 port detected

Initializing USB Mass Storage driver...

usbcore: registered new interface driver usb-storage

USB Mass Storage support registered.

ARC USBOTG Device Controller driver (1 August 2005)

mousedev: PS/2 mouse device common for all mice

input: gpio-keys as /devices/platform/gpio-keys/input/input0

input: max11801_ts as /devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1

egalax_ts 1-0004: egalax_ts: failed to read firmware version

egalax_ts: probe of 1-0004 failed with error -5

input: eGalax Touch Screen as /devices/platform/imx-i2c.2/i2c-2/2-0004/input/input2

elan - Read Hello Packet Failed

elan-touch: probe of 2-0010 failed with error -22

input: isl29023 light sensor as /devices/virtual/input/input3

isl29023 2-0044: driver version 1.0 enabled

i2c-core: driver [isl29023] using legacy suspend method

i2c-core: driver [isl29023] using legacy resume method

snvs_rtc snvs_rtc.0: rtc core: registered snvs_rtc as rtc0

i2c /dev entries driver

Linux video capture interface: v2.00

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video16

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video17

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video18

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video19

mxc_v4l2_output mxc_v4l2_output.0: V4L2 device registered as video20

mag3110 2-000e: check mag3110 chip ID

input: mag3110 as /devices/virtual/input/input4

mag3110 2-000e: mag3110 is probed

i2c-core: driver [mag3110] using legacy suspend method

i2c-core: driver [mag3110] using legacy resume method

input: mma845x as /devices/virtual/input/input5

imx2-wdt imx2-wdt.0: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=1)

Bluetooth: Virtual HCI driver ver 1.3

Bluetooth: HCI UART driver ver 2.2

Bluetooth: HCIATH3K protocol initialized

Bluetooth: Generic Bluetooth USB driver ver 0.6

usbcore: registered new interface driver btusb

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

mmc0: SDHCI controller on platform [sdhci-esdhc-imx.3] using DMA

mmc1: SDHCI controller on platform [sdhci-esdhc-imx.1] using DMA

mmc2: SDHCI controller on platform [sdhci-esdhc-imx.2] using DMA

mxc_vdoa mxc_vdoa: i.MX Video Data Order Adapter(VDOA) driver probed

VPU initialized

mxc_asrc registered

Thermal calibration data is 0x5744b57d

Anatop Thermal registered as thermal_zone0

anatop_thermal_probe: default cooling device is cpufreq!

caam caam.0: device ID = 0x0a16010000000000

caam caam.0: job rings = 2, qi = 0

alg: No test for authenc(hmac(md5),cbc(aes)) (authenc-hmac-md5-cbc-aes-caam)

caam caam.0: authenc-hmac-md5-cbc-aes-caam

alg: No test for authenc(hmac(sha1),cbc(aes)) (authenc-hmac-sha1-cbc-aes-caam)

caam caam.0: authenc-hmac-sha1-cbc-aes-caam

alg: No test for authenc(hmac(sha224),cbc(aes)) (authenc-hmac-sha224-cbc-aes-caam)

caam caam.0: authenc-hmac-sha224-cbc-aes-caam

alg: No test for authenc(hmac(sha256),cbc(aes)) (authenc-hmac-sha256-cbc-aes-caam)

caam caam.0: authenc-hmac-sha256-cbc-aes-caam

alg: No test for authenc(hmac(md5),cbc(des3_ede)) (authenc-hmac-md5-cbc-des3_ede-caam)

caam caam.0: authenc-hmac-md5-cbc-des3_ede-caam

alg: No test for authenc(hmac(sha1),cbc(des3_ede)) (authenc-hmac-sha1-cbc-des3_ede-caam)

caam caam.0: authenc-hmac-sha1-cbc-des3_ede-caam

alg: No test for authenc(hmac(sha224),cbc(des3_ede)) (authenc-hmac-sha224-cbc-des3_ede-caam)

caam caam.0: authenc-hmac-sha224-cbc-des3_ede-caam

alg: No test for authenc(hmac(sha256),cbc(des3_ede)) (authenc-hmac-sha256-cbc-des3_ede-caam)

caam caam.0: authenc-hmac-sha256-cbc-des3_ede-caam

alg: No test for authenc(hmac(md5),cbc(des)) (authenc-hmac-md5-cbc-des-caam)

caam caam.0: authenc-hmac-md5-cbc-des-caam

alg: No test for authenc(hmac(sha1),cbc(des)) (authenc-hmac-sha1-cbc-des-caam)

caam caam.0: authenc-hmac-sha1-cbc-des-caam

alg: No test for authenc(hmac(sha224),cbc(des)) (authenc-hmac-sha224-cbc-des-caam)

caam caam.0: authenc-hmac-sha224-cbc-des-caam

mmc0: new high speed DDR MMC card at address 0001

mmcblk0: mmc0:0001 SEM08G 7.39 GiB

mmcblk0boot0: mmc0:0001 SEM08G partition 1 2.00 MiB

mmcblk0boot1: mmc0:0001 SEM08G partition 2 2.00 MiB

mmcblk0: unknown partition table

alg: No test for authenc(hmac(sha256),cbc(des)) (authenc-hmac-sha256-cbc-des-caam)

mmcblk0boot1: unknown partition table

caam caam.0: authenc-hmac-sha256-cbc-des-caam

mmcblk0boot0: unknown partition table

caam caam.0: cbc-aes-caam

caam caam.0: cbc-3des-caam

caam caam.0: cbc-des-caam

platform caam_jr.0: registering rng-caam

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

usbcore: registered new interface driver snd-usb-audio

mxc_hdmi_soc mxc_hdmi_soc.0: MXC HDMI Audio

Cirrus Logic CS42888 ALSA SoC Codec Driver

i2c-core: driver [cs42888] using legacy suspend method

i2c-core: driver [cs42888] using legacy resume method

wm8962 0-001a: customer id 0 revision D

input: WM8962 Beep Generator as /devices/platform/imx-i2c.0/i2c-0/0-001a/input/input6

asoc: wm8962 <-> imx-ssi.1 mapping ok

imx_3stack asoc driver

imx-hdmi-soc-dai: probe of imx-hdmi-soc-dai.0 failed with error -12

ALSA device list:

  #0: wm8962-audio

mmc2: new high speed SDHC card at address b368

NET: Registered protocol family 26

TCP cubic registered

NET: Registered protocol family 17

can: controller area network core (rev 20090105 abi 8)

mmcblk1: mmc2:b368 USD   3.75 GiB

NET: Registered protocol family 29

can: raw protocol (rev 20090105)

mmcblk1: p1 p2

can: broadcast manager protocol (rev 20090105 t)

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

lib80211: common routines for IEEE802.11 drivers

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

Bus freq driver module loaded

Bus freq driver Enabled

mxc_dvfs_core_probe

DVFS driver module loaded

regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on

regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on

regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on

regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on

regulator_init_complete: vddpu: incomplete constraints, leaving on

snvs_rtc snvs_rtc.0: setting system clock to 2013-05-17 09:19:46 UTC (1368782386)

EXT3-fs: barriers not enabled

kjournald starting.  Commit interval 5 seconds

EXT3-fs (mmcblk1p2): using internal journal

EXT3-fs (mmcblk1p2): recovery complete

EXT3-fs (mmcblk1p2): mounted filesystem with writeback data mode

VFS: Mounted root (ext3 filesystem) on device 179:26.

devtmpfs: mounted

Freeing init memory: 204K

INIT: version 2.88 booting

Starting udev

udevd[130]: starting version 182

Starting Bootlog daemon: bootlogd.

ALSA: Restoring mixer settings...

No state is present for card wm8962audio

Found hardware: "wm8962-audio" "" "" "" ""

Hardware is initialized using a generic method

Configuring network interfaces... No state is present for card wm8962audio

eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:01, irq=-1)

udhcpc (v1.20.2) started

Sending discover...

Sending discover...

Sending discover...

No lease, failing

Starting rpcbind daemon...rpcbind: cannot create socket for udp6

rpcbind: cannot create socket for tcp6

done.

INIT: Entering runlevel: 5

Starting Xserver

Starting system message bus: dbus.

Starting advanced power management daemon: apmd.

apmd[642]: apmd 3.2.1 interfacing with apm driver 1.13 and APM BIOS 1.2

Starting syslogd/klogd: done

* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon

   ...done.

Starting Telephony daemon

Starting Linux NFC daemon

imx-audio: setting default mixer settings.

amixer: Unable to find simple control 'Speaker Function',0

amixer: Unable to find simple control 'Playback',0

amixer: Unable to find simple control 'Jack Function',0

Stopping Bootlog daemon: bootlogd.

Poky 9.0 (Yocto Project 1.4 Reference Distro) 1.4 imx6qsabresd ttymxc0

imx6qsabresd login:

The x-server is running, as it is shown in ps and there is no error in the /var/log/Xorg.0.log, but no output on the 10" screen.

I have the same issue using Yocto-danny, nothing on the screen.

Can anybody help me, please?







标签 (4)
标记 (1)
1 解答
2,039 次查看
LeonardoSandova
Specialist I

As a last try, connect the screen into the toher LVDS port or add ldb=dul0/1  into the kernel cmd line. If issue persists, post this into the meta-freescale mailing list.

Leo

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,039 次查看
varsmolta
Contributor V

you may need to give kernel args for enabling the display. It will either be mmcargs or bootargs (depending on your boot medium). Look here for details:

https://community.freescale.com/message/319071#319071

0 项奖励
回复
2,039 次查看
c_hahn
Contributor III

I already tried this with extending the mmcargs with

video=mxcfb0:dev=ldb,LDB-XGA,if=RGB666

as well as

video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666

but no change.

By the way,  the kernel that comes with the new L3.0.35_4.0.0_DEMO_IMAGE did not need any additional kernel bootarg to enable the 10" display.

0 项奖励
回复
2,040 次查看
LeonardoSandova
Specialist I

As a last try, connect the screen into the toher LVDS port or add ldb=dul0/1  into the kernel cmd line. If issue persists, post this into the meta-freescale mailing list.

Leo

0 项奖励
回复
2,039 次查看
c_hahn
Contributor III

YES, this was the missing part! Just adding ldb=dul0 did it.

The video=mxcfb1:dev=ldb,LDB-XGA,if=RGB666 is not needed.

Thanks a lot.

0 项奖励
回复