error when enable systemd in swupdate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error when enable systemd in swupdate

2,018件の閲覧回数
wang12zhe
Contributor III

HW :IMX8QXP EVK

Yocto :5.10.52

Step 1 : Enable systemd support in swupdate:

           bitbke -c menuconfig swupdate

             Swupdate Setting--->

                 General Configuration---->

                     enable systemd support

Step2: bitbake swupdate,will show error :

 

| /home/wzg/8TB/Yocto/L5.10.52/build-xwayland/tmp/work/cortexa35-poky-linux/swupdate/2021.11-r0/git/core/notifier.c:27:10: fatal error: systemd/sd-daemon.h: No such file or directory
| 27 | #include <systemd/sd-daemon.h>
| | ^~~~~~~~~~~~~~~~~~~~~
| compilation terminated.
| make[2]: *** [/home/wzg/8TB/Yocto/L5.10.52/build-xwayland/tmp/work/cortexa35-poky-linux/swupdate/2021.11-r0/git/scripts/Makefile.build:168: core/notifier.o] Error 1
| make[2]: *** Waiting for unfinished jobs....
| /home/wzg/8TB/Yocto/L5.10.52/build-xwayland/tmp/work/cortexa35-poky-linux/swupdate/2021.11-r0/git/core/swupdate.c:53:10: fatal error: systemd/sd-daemon.h: No such file or directory
| 53 | #include <systemd/sd-daemon.h>
| | ^~~~~~~~~~~~~~~~~~~~~
| compilation terminated.
| make[2]: *** [/home/wzg/8TB/Yocto/L5.10.52/build-xwayland/tmp/work/cortexa35-poky-linux/swupdate/2021.11-r0/git/scripts/Makefile.build:168: core/swupdate.o] Error 1
| /home/wzg/8TB/Yocto/L5.10.52/build-xwayland/tmp/work/cortexa35-poky-linux/swupdate/2021.11-r0/git/core/network_thread.c:37:10: fatal error: systemd/sd-daemon.h: No such file or directory
| 37 | #include <systemd/sd-daemon.h>
| | ^~~~~~~~~~~~~~~~~~~~~
| compilation terminated.
| make[2]: *** [/home/wzg/8TB/Yocto/L5.10.52/build-xwayland/tmp/work/cortexa35-poky-linux/swupdate/2021.11-r0/git/scripts/Makefile.build:168: core/network_thread.o] Error 1
| make[1]: *** [/home/wzg/8TB/Yocto/L5.10.52/build-xwayland/tmp/work/cortexa35-poky-linux/swupdate/2021.11-r0/git/Makefile:515: core] Error 2
| make[1]: *** Waiting for unfinished jobs....
| make: *** [Makefile:97: sub-make] Error 2
| WARNING: exit code 1 from a shell command.

 

How to fix the error :

fatal error: systemd/sd-daemon.h: No such file or directory

            

 

 

0 件の賞賛
返信
1 返信

1,999件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

FYI. You could follow the steps in AN13872 to build the swupdate.

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/SWUpdate-OTA-i-MX8MM-EVK-i-MX8QXP-MEK/ta...

 

0 件の賞賛
返信