eMMC5.0 Boot with Bus Width=8bit access for i.MX6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eMMC5.0 Boot with Bus Width=8bit access for i.MX6

1,241 次查看
rahulsoni
Contributor II

Hi All,

We have one custom i.MX6S board which we are booting using eMMC.

I can see no difference in booting time when I set boot_cfg2[7:5] = 000 (1 bit) and boot_cfg2[7:5] = 010 (8 bit).

Can anyone please explain why this is happening. Ideally, when selecting 1-bit eMMC, booting time should be more than 8-bit booting time.

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

982 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Rahul

emmc has internal non-volatile configuration register for bus width :

EXT_CSD [177] BOOT_BUS_WIDTH, which also should be programmed appropriately.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复