freezes during boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

freezes during boot

2,002 Views
borune
Contributor I

hi again,
i've faced with such problem. I have a imx6solo board with linux.There is gstreamer daemon, running from /etc/rc3 during os booting. I've edited gstreamer daemon params and entered invalid parameter, saved daemon conffile and rebooted board. After booting i get about 5 seconds (i can see gstreamer error caused by invalid parameter) for doing anything, after that os is freezes. Only hard reset can help, but after booting it repeats again. Finally board stoped booting at all. It don't give me any messages to putty. What should i do? How can i reanimate my board?

0 Kudos
Reply
1 Reply

1,934 Views
igorpadykov
NXP Employee
NXP Employee

Hi Boris

one can try to make new sd card using attached Linux Guide or MFG Tool

http://www.nxp.com/webapp/Download?colCode=IMX6_L4-1-15_2-0-0_MFG-TOOL&appType=license&location=null... 

more documentation is available on

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply