eMMC5.0 Boot with Bus Width=8bit access for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC5.0 Boot with Bus Width=8bit access for i.MX6

1,263 Views
rahulsoni
Contributor II

Hi All,

We have one custom i.MX6S board which we are booting using eMMC.

I can see no difference in booting time when I set boot_cfg2[7:5] = 000 (1 bit) and boot_cfg2[7:5] = 010 (8 bit).

Can anyone please explain why this is happening. Ideally, when selecting 1-bit eMMC, booting time should be more than 8-bit booting time.

Labels (1)
0 Kudos
Reply
1 Reply

1,004 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rahul

emmc has internal non-volatile configuration register for bus width :

EXT_CSD [177] BOOT_BUS_WIDTH, which also should be programmed appropriately.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply