eMMC request timeut error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC request timeut error

2,923 Views
nishadkamdar
Contributor III

We have a custom IMX8MM board with a 4GB eMMC chip connected.

We see the following error while emmc read/write test on the eMMC device:

mmc0: request with tag: 16 flags: 0x2000000002469030 timed out

Can anyone suggest why this timeout may have occurred ?

Thanks for the continued support.

Regards,

Nishad

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

2,874 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

     You can try to add the following member to device tree:

---------------------

     no-1-8-v;

----------------------

     Then try.

Have a  nice day!

B.R,

Weidong

0 Kudos
Reply

2,913 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

i.MX8MM EMMC has never encountered such a problem, and you need to provide the following detailed information:

1. Is the customer's EMMC 1.8V IO or 3.3V IO?

2. Is the customer using LPDDR4 or DDR4?

3. Can the board start normally?

4. If possible, please provide the pdf schematic diagram and linux startup log.

Have a nice day!

B.R,

weidong

0 Kudos
Reply

2,883 Views
nishadkamdar
Contributor III

Hello,

Thanks for the quick reply.

The customer eMMC is 1.8v. It uses LPDDR4 and the board boots fine as well.

Sorry cannot share the schematic for privacy reasons.

The error also seems related to command queue.

mmc_blk_cmdq_err err

 

Thanks and regards,

Nishad

 

 

0 Kudos
Reply

2,801 Views
Stefan_ng
Contributor II

Hi Nishad,

Have you solved the problem?

If hopefully yes, the question is how?

Thank you,

Stefan

0 Kudos
Reply