eMMC request timeut error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMC request timeut error

2,890件の閲覧回数
nishadkamdar
Contributor III

We have a custom IMX8MM board with a 4GB eMMC chip connected.

We see the following error while emmc read/write test on the eMMC device:

mmc0: request with tag: 16 flags: 0x2000000002469030 timed out

Can anyone suggest why this timeout may have occurred ?

Thanks for the continued support.

Regards,

Nishad

ラベル(1)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

2,841件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

     You can try to add the following member to device tree:

---------------------

     no-1-8-v;

----------------------

     Then try.

Have a  nice day!

B.R,

Weidong

0 件の賞賛
返信

2,880件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

i.MX8MM EMMC has never encountered such a problem, and you need to provide the following detailed information:

1. Is the customer's EMMC 1.8V IO or 3.3V IO?

2. Is the customer using LPDDR4 or DDR4?

3. Can the board start normally?

4. If possible, please provide the pdf schematic diagram and linux startup log.

Have a nice day!

B.R,

weidong

0 件の賞賛
返信

2,850件の閲覧回数
nishadkamdar
Contributor III

Hello,

Thanks for the quick reply.

The customer eMMC is 1.8v. It uses LPDDR4 and the board boots fine as well.

Sorry cannot share the schematic for privacy reasons.

The error also seems related to command queue.

mmc_blk_cmdq_err err

 

Thanks and regards,

Nishad

 

 

0 件の賞賛
返信

2,768件の閲覧回数
Stefan_ng
Contributor II

Hi Nishad,

Have you solved the problem?

If hopefully yes, the question is how?

Thank you,

Stefan

0 件の賞賛
返信