eMMC performance testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eMMC performance testing

ソリューションへジャンプ
15,154件の閲覧回数
nirmalluhana
Contributor IV

Hi,

 

Release: Yocto-Morty (4.9.51_GA)

Board: i.MX8MQ EVK

I have tested eMMC performance on iMX8MQ EVK board using dd & hdparm and I observed that read speed is approx 135-140 MB/s and write speed is approx 20 MB/s. While referring eMMC datasheet it mentions that eMMC performance as below image.

Screenshot from 2019-01-29 15-34-19.png

So, what is the reason I have got that much low performance?

Best regards,

Nirmal

ラベル(1)
1 解決策
14,050件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

slow emmc write issues were already reported on web, like

Re: slow eMMC write speed — Linux MMC Development 

In particular below presentation emphasize on write performance issues for this type of media.

https://elinux.org/images/4/41/Linux_on_eMMC-_Optimizing_For_Performance.pdf 

As for i.MX8MQ, it has many modules and complex architecture with bus arbiters,

so it is not possible to provide max. performance characteristics for every module.

You can increase performance for one module, but that may affect others.

General answer is provided on

USB 3.0 Raw Throughput 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

5 返答(返信)
6,156件の閲覧回数
Robbi
Contributor III

Hi @nirmalluhana ,

                          I'm using imx8, can you help with user manual or commands to test eMMC. 

 

 

Thanks & Regards 

Robbi

タグ(1)
0 件の賞賛
返信
14,051件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nirmal

slow emmc write issues were already reported on web, like

Re: slow eMMC write speed — Linux MMC Development 

In particular below presentation emphasize on write performance issues for this type of media.

https://elinux.org/images/4/41/Linux_on_eMMC-_Optimizing_For_Performance.pdf 

As for i.MX8MQ, it has many modules and complex architecture with bus arbiters,

so it is not possible to provide max. performance characteristics for every module.

You can increase performance for one module, but that may affect others.

General answer is provided on

USB 3.0 Raw Throughput 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

14,050件の閲覧回数
nirmalluhana
Contributor IV

Hi Igor,

Thanks for your quick support. I understood the reason why it was happening.

Best regards,

Nirmal 

0 件の賞賛
返信
10,848件の閲覧回数
jagsgediya
Contributor II

Hi @nirmalluhana What was the reason for slow performance?

0 件の賞賛
返信
10,662件の閲覧回数
chen-wust
Contributor II

Now I also want to improve the read and write speed of emmc. Do you have any progress

0 件の賞賛
返信