OS08A20 camera and LVDS touch display support on iMX 95 Verdin EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OS08A20 camera and LVDS touch display support on iMX 95 Verdin EVK

1,077 Views
pion3k_vk
Contributor I

Hi, I am verifying camera and touch display support on the iMX 95 Verdin EVK with the NXP Android 14.0.0 2.2.0 release (Rev. android-14.0.0_2.2.0 — 18 October 2024) and I have some concerns about the available support for certain features.

1. Capacitive Touch Display 10.1" LVDS support

Does the NXP Android 14 2.2.0 release build support 'touch' functionality for the 10" LVDS capacitive touch display? I flashed the EVK with -d verdin-10inch-panel-lvds option and after connecting the LVDS cable + 10 Pins 0.5mm FFC Ribbon Cable to the EVK the display itself is working but the 'touch' functionality isn't (although the FFC ribbon cable seems to be connected properly according to the Toradex documentation for the above display).

2. OS08A20 camera support

Is it feasible to flash the Android build witch such device-tree which would support both the LVDS display and 4K MIPI CMOS Camera Module? Or at least MIPI-to-HDMI (LT8912) display + camera?

BR
Marek

0 Kudos
Reply
2 Replies

1,000 Views
pion3k_vk
Contributor I

Thanks but the Android OS, if I understand it correctly, is released by NXP here: https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/android-os-for-i-m... and I am referring to this particular software (Android 14 2.2.0). 

BR 
Marek 

0 Kudos
Reply

1,044 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @pion3k_vk!
Thank you for contacting NXP Support!

 

At the moment all the documentation available for the iMX95 is confidential.

We don't support the board that you are using due to we don't provide the software for this board, please contact to Toradex Support for this case

 

Best Regards!

Chavira

0 Kudos
Reply