eLCDIF synchronization with external clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eLCDIF synchronization with external clock

1,302件の閲覧回数
rickburnett
Contributor I

If I understand the user guide correctly, it would appear that we can set PLL5 (Video PLL) to Bypass mode and have it listen to external clock CLK_N/CLK_P instead.  While I understand we can use a VSYNC with the eLCDIF VSYNC mode, we want to actually synchronize the pixel clock as well which there is no input I can see for that, unless I am mistaken.

Does this sound correct?

0 件の賞賛
返信
1 返信

1,255件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rick

yes this is correct, PLL can be bypassed and use external clock CLK_N/CLK_P

instead. There is no option in eLCDIF module for exaternal pixel clock.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信