dynamic/changeable boot command line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

dynamic/changeable boot command line

ソリューションへジャンプ
2,878件の閲覧回数
chris321
Contributor IV

Hello community,

I want to use the imx28evk with an 2.6.35 Kernel.

I know how I can change the Linux kernel boot command line and this requires a rebuild of the boot stream.

But now I want to change the boot command line out of the target, like in a desktop linux a grub/lilo config file.

The goal of this is, that we can change the boot stream and the rootfs dynamically.

Is this possible (with/without) uboot?

best regards


ラベル(2)
0 件の賞賛
返信
1 解決策
2,707件の閲覧回数
JackyAtFreescal
Senior Contributor II

From my understanding, the kernel command line cannot be changed at run time for i.MX28.

https://community.nxp.com/message/312802/edit" style="font-style: inherit; font-family: inherit; col...

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,707件の閲覧回数
YixingKong
Senior Contributor IV

Chris321, did Jacky1z answer your question? If yes, please click Correct Answer button, so that your DI will be closed.

Thanks,

0 件の賞賛
返信
2,708件の閲覧回数
JackyAtFreescal
Senior Contributor II

From my understanding, the kernel command line cannot be changed at run time for i.MX28.

https://community.nxp.com/message/312802/edit" style="font-style: inherit; font-family: inherit; col...

0 件の賞賛
返信