dynamic/changeable boot command line

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

dynamic/changeable boot command line

Jump to solution
2,916 Views
chris321
Contributor IV

Hello community,

I want to use the imx28evk with an 2.6.35 Kernel.

I know how I can change the Linux kernel boot command line and this requires a rebuild of the boot stream.

But now I want to change the boot command line out of the target, like in a desktop linux a grub/lilo config file.

The goal of this is, that we can change the boot stream and the rootfs dynamically.

Is this possible (with/without) uboot?

best regards


Labels (2)
0 Kudos
Reply
1 Solution
2,745 Views
JackyAtFreescal
Senior Contributor II

From my understanding, the kernel command line cannot be changed at run time for i.MX28.

https://community.nxp.com/message/312802/edit" style="font-style: inherit; font-family: inherit; col...

View solution in original post

0 Kudos
Reply
2 Replies
2,745 Views
YixingKong
Senior Contributor IV

Chris321, did Jacky1z answer your question? If yes, please click Correct Answer button, so that your DI will be closed.

Thanks,

0 Kudos
Reply
2,746 Views
JackyAtFreescal
Senior Contributor II

From my understanding, the kernel command line cannot be changed at run time for i.MX28.

https://community.nxp.com/message/312802/edit" style="font-style: inherit; font-family: inherit; col...

0 Kudos
Reply