- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
hello
i have an encrypted partition with dm-crypt. on first boot all seems well but after i burn my applications, not always but accusingly, some of my files get corrupted. also after running for some time i also get some of my files corrupted.
before creating a dm-crypt partition, on a normal partition i never got corrupted files.
is there a reason why the encrypted partition is not stable
thanks for the help
解決済! 解決策の投稿を見る。
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi
i was able to find the problem, i was directed to the solution by Nathan from Timesys. it seems there is a bug in the crypto dirver backlog scenario
thanks
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi,
Thank you for your interest in NXP Semiconductor products,
Could you share how could I reproduce this issue?
Please confirm if you are following the steps from this guide, this may help out.
Also, what processor are you working with?
Regards
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
hi
i also tested the partition with the test in the manual and got errors. the first test is on a normal partition and second test is on an encrypted partition
dd if=/dev/random of=/tmp/random conv=fsync bs=1M count=32
32+0 records in
32+0 records out
33554432 bytes (34 MB, 32 MiB) copied, 0.335412 s, 100 MB/s
root@imx8mp-var-dart-aion-secure:~# echo 3 > /proc/sys/vm/drop_caches
[ 853.846594] sh (582): drop_caches: 3
---- testing on a normal partition --
root@imx8mp-var-dart-aion-secure:~# time dd if=/tmp/random of=/home/root/testwrite conv=fsync
65536+0 records in
65536+0 records out
33554432 bytes (34 MB, 32 MiB) copied, 0.805649 s, 41.6 MB/s
real 0m0.818s
user 0m0.055s
sys 0m0.643s
root@imx8mp-var-dart-aion-secure:~# rm testwrite
--- testing in the encrypted partition ---
root@imx8mp-var-dart-aion-secure:~# time dd if=/tmp/random of=/data/testwrite conv=fsync
[ 886.872817] caam_jr 30902000.jr: swiotlb buffer is full (sz: 512 bytes), total 32768 (slots), used 32767 (slots)
[ 886.873141] caam_jr 30902000.jr: swiotlb buffer is full (sz: 512 bytes), total 32768 (slots), used 32768 (slots)
[ 886.873144] sdhci-esdhc-imx 30b60000.mmc: swiotlb buffer is full (sz: 8192 bytes), total 32768 (slots), used 32766 (slots)
[ 886.874542] sdhci-esdhc-imx 30b60000.mmc: swiotlb buffer is full (sz: 8192 bytes), total 32768 (slots), used 32766 (slots)
[ 886.874608] ------------[ cut here ]------------
[ 886.874611] WARNING: CPU: 0 PID: 210 at drivers/mmc/host/sdhci.c:1154 sdhci_send_command+0x7e8/0xe6c
[ 886.874625] Modules linked in: iptable_filter ip_tables x_tables crct10dif_ce imx8_media_dev(C) imx_sdma secvio fsl_jr_uio snd_soc_wm8904 imx_rpmsg_tty galcore(O) fuse
[ 886.874656] CPU: 0 PID: 210 Comm: kworker/0:1H Tainted: G WC O 5.15.71+gd567aaeb594f #1
[ 886.874662] Hardware name: DART-MX8M-PLUS Elsec Aion (DT)
[ 886.874666] Workqueue: kblockd blk_mq_run_work_fn
[ 886.874676] pstate: a00000c5 (NzCv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 886.874682] pc : sdhci_send_command+0x7e8/0xe6c
[ 886.874686] lr : sdhci_send_command+0x648/0xe6c
[ 886.874690] sp : ffff80000ae3b960
[ 886.874692] x29: ffff80000ae3b960 x28: 0000000000000000 x27: 0000000000000002
[ 886.874700] x26: 0000000000000000 x25: 0000000000000000 x24: ffff0000c0f38810
[ 886.874708] x23: 000000000000000b x22: ffff0000c53db348 x21: ffff0000c53db3b8
[ 886.874716] x20: ffff0000c53db348 x19: ffff0000c0f38580 x18: ffffffffffffffff
[ 886.874724] x17: 0000000000000000 x16: 00000000302abb46 x15: ffff800009f61fc0
[ 886.874731] x14: ffffffffffffffff x13: ffff800009f61fb1 x12: 7566207369207265
[ 886.874739] x11: ffff800009dd2100 x10: 0000000000000020 x9 : 0000000000007ffe
[ 886.874747] x8 : 0000000000000020 x7 : 000000000000003a x6 : 0000000000007940
[ 886.874754] x5 : ffff0000fb1a5d88 x4 : 0000000000000000 x3 : 0000000000000000
[ 886.874761] x2 : fffffffffffdfbfe x1 : fffffffffffffffe x0 : 00000000ffffffe4
[ 886.874770] Call trace:
[ 886.874772] sdhci_send_command+0x7e8/0xe6c
[ 886.874777] sdhci_send_command_retry+0x40/0x130
[ 886.874782] sdhci_request+0x70/0xc4
[ 886.874786] __mmc_start_request+0x68/0x13c
[ 886.874793] mmc_start_request+0x84/0xb0
[ 886.874799] mmc_blk_mq_issue_rq+0x310/0xa70
[ 886.874805] mmc_mq_queue_rq+0x11c/0x2bc
[ 886.874811] blk_mq_dispatch_rq_list+0x124/0x83c
[ 886.874817] blk_mq_do_dispatch_sched+0x2a4/0x320
[ 886.874822] __blk_mq_sched_dispatch_requests+0x10c/0x15c
[ 886.874827] blk_mq_sched_dispatch_requests+0x38/0x74
[ 886.874832] __blk_mq_run_hw_queue+0x54/0x90
[ 886.874837] blk_mq_run_work_fn+0x20/0x30
[ 886.874843] process_one_work+0x1d0/0x354
[ 886.874848] worker_thread+0x13c/0x470
[ 886.874852] kthread+0x150/0x160
[ 886.874857] ret_from_fork+0x10/0x20
[ 886.874864] ---[ end trace e71339d44b27c803 ]---
[ 886.883023] caam_jr 30902000.jr: unable to map destination
[ 886.891124] caam_jr 30902000.jr: swiotlb buffer is full (sz: 512 bytes), total 32768 (slots), used 32768 (slots)
[ 886.891974] caam_jr 30902000.jr: swiotlb buffer is full (sz: 512 bytes), total 32768 (slots), used 32768 (slots)
[ 886.891982] caam_jr 30902000.jr: unable to map source
[ 886.892000] caam_jr 30902000.jr: swiotlb buffer is full (sz: 512 bytes), total 32768 (slots), used 32768 (slots)
[ 886.892006] caam_jr 30902000.jr: unable to map source
[ 886.892135] caam_jr 30902000.jr: swiotlb buffer is full (sz: 512 bytes), total 32768 (slots), used 32768 (slots)
[ 886.892140] caam_jr 30902000.jr: unable to map source
[ 886.892192] EXT4-fs warning (device dm-1): ext4_end_bio:344: I/O error 10 writing to inode 14 starting block 763715)
[ 886.892325] caam_jr 30902000.jr: swiotlb buffer is full (sz: 512 bytes), total 32768 (slots), used 32768 (slots)
[ 886.892331] caam_jr 30902000.jr: unable to map source
[ 886.892513] caam_jr 30902000.jr: swiotlb buffer is full (sz: 512 bytes), total 32768 (slots), used 32768 (slots)
[ 886.892518] caam_jr 30902000.jr: unable to map source
[ 886.892701] caam_jr 30902000.jr: unable to map source
[ 886.892828] caam_jr 30902000.jr: unable to map source
[ 886.892864] EXT4-fs warning (device dm-1): ext4_end_bio:344: I/O error 10 writing to inode 14 starting block 764672)
[ 886.892985] caam_jr 30902000.jr: unable to map source
[ 886.893167] caam_jr 30902000.jr: unable to map source
[ 886.893274] caam_jr 30902000.jr: unable to map source
[ 886.893350] caam_jr 30902000.jr: unable to map source
[ 886.893533] caam_jr 30902000.jr: unable to map source
[ 886.893623] caam_jr 30902000.jr: unable to map source
[ 886.893652] EXT4-fs warning (device dm-1): ext4_end_bio:344: I/O error 10 writing to inode 14 starting block 765819)
[ 886.893705] caam_jr 30902000.jr: unable to map source
[ 886.893737] EXT4-fs warning (device dm-1): ext4_end_bio:344: I/O error 10 writing to inode 14 starting block 765863)
[ 886.893873] caam_jr 30902000.jr: unable to map source
[ 886.894001] Buffer I/O error on device dm-1, logical block 765863
[ 886.894025] Buffer I/O error on device dm-1, logical block 765864
[ 886.894030] Buffer I/O error on device dm-1, logical block 765865
[ 886.894035] Buffer I/O error on device dm-1, logical block 765866
[ 886.894039] Buffer I/O error on device dm-1, logical block 765867
[ 886.894044] Buffer I/O error on device dm-1, logical block 765868
[ 886.894048] Buffer I/O error on device dm-1, logical block 765869
[ 886.894052] Buffer I/O error on device dm-1, logical block 765870
[ 886.894057] Buffer I/O error on device dm-1, logical block 765871
[ 886.894061] Buffer I/O error on device dm-1, logical block 765872
[ 886.897488] caam_jr 30902000.jr: unable to map source
[ 886.897683] caam_jr 30902000.jr: unable to map source
[ 886.897868] caam_jr 30902000.jr: unable to map source
[ 886.898052] caam_jr 30902000.jr: unable to map source
[ 886.898236] caam_jr 30902000.jr: unable to map source
[ 886.898335] caam_jr 30902000.jr: unable to map source
[ 886.898359] EXT4-fs warning (device dm-1): ext4_end_bio:344: I/O error 10 writing to inode 14 starting block 755200)
[ 886.898481] caam_jr 30902000.jr: unable to map source
[ 886.898634] caam_jr 30902000.jr: unable to map source
[ 886.898685] EXT4-fs warning (device dm-1): ext4_end_bio:344: I/O error 10 writing to inode 14 starting block 755523)
[ 886.920412] caam_jr 30902000.jr: unable to map destination
[ 887.193383] EXT4-fs warning (device dm-1): ext4_end_bio:344: I/O error 10 writing to inode 14 starting block 763181)
[ 887.455933] EXT4-fs warning (device dm-1): ext4_end_bio:344: I/O error 10 writing to inode 14 starting block 763711)
dd: fsync failed for '/data/testwrite': Input/output error
65536+0 records in
65536+0 records out
33554432 bytes (34 MB, 32 MiB) copied, 1.43458 s, 23.4 MB/s
real 0m1.442s
user 0m0.060s
sys 0m0.661s
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi
i was able to find the problem, i was directed to the solution by Nathan from Timesys. it seems there is a bug in the crypto dirver backlog scenario
thanks
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
Hi,
Thanks for the inputs,
There shouldn't be reason to be unstable, let me try to replicate the issue.
Regards,
Joseph
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
where you able to replicate the issue
thanks
Ran
- 新着としてマーク
- ブックマーク
- 購読
- ミュート
- RSS フィードを購読する
- ハイライト
- 印刷
- 不適切なコンテンツを報告
hi
thanks for the quick response. i am creating the partition and mounting it in the initramfs. the creation and mount are the same commands as the manual. The create has --verifyudev parameter. When i run the "dmsetup table --showkey" on the partitions that are encrypted i get a similar result as the manual.
is there any reason why the dm-crypt should be unstable ?
thanks