configuring the resolution of display in boot command line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

configuring the resolution of display in boot command line

ソリューションへジャンプ
2,325件の閲覧回数
jojorong
Contributor IV

Hi,

  How to know that how many resolution supported in current device with HDMI output (my device is imx6q) ?

root@imx6qsabresd:/# find -name modes

./sys/devices/platform/mxc_sdc_fb.0/graphics/fb0/modes

./sys/devices/platform/mxc_sdc_fb.0/graphics/fb1/modes

./sys/devices/platform/mxc_sdc_fb.1/graphics/fb2/modes

./sys/devices/platform/mxc_sdc_fb.1/graphics/fb3/modes

./sys/devices/platform/mxc_sdc_fb.3/graphics/fb4/modes

root@imx6qsabresd:/# cat ./sys/devices/platform/mxc_sdc_fb.0/graphics/fb0/modes

V:640x480p-60

D:1920x1080p-60

U:640x480p-60

0 件の賞賛
返信
1 解決策
1,828件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

yes.

First time I replied I pasted the wrong URL. Then I did edit my reply. I think you was not notified via email. Please see this:

https://community.freescale.com/thread/306901

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,828件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Sorry, I did not understand your goal

0 件の賞賛
返信
1,828件の閲覧回数
jojorong
Contributor IV

Hi,

I want to configure resolution 1366x768 about for HDMI output in the 6Q, may i ?

Thanks,

- Jojo

在 2013年6月25日星期二,上午12:55,Daiane Angolini 写道:

configuring the resolution of display in boot command line

created by Daiane Angolini (https://community.freescale.com/people/DaianeAngolini) in i.MX Community - View the full discussion (https://community.freescale.com/message/336482#336482)

Sorry, I did not understand your goal

Reply to this message by replying to this email -or- go to the message on Freescale Community (https://community.freescale.com/message/336482#336482)

Start a new discussion in i.MX Community by email (mailto:discussions-community-imx@freescale-phx.hosted.jivesoftware.com ) or at Freescale Community (https://community.freescale.com/choose-container.jspa?contentType=1&containerType=14&container=2004)

>

0 件の賞賛
返信
1,828件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Sure, please follow this thread:

https://community.freescale.com/thread/306901

0 件の賞賛
返信
1,828件の閲覧回数
jojorong
Contributor IV

Hi,

I have no permit to see anything about for the following thread, have any ideas ?

https://community.freescale.com/thread/306944

Thanks,

- Jojo

在 2013年6月26日星期三,上午12:57,Daiane Angolini 写道:

configuring the resolution of display in boot command line

created by Daiane Angolini (https://community.freescale.com/people/DaianeAngolini) in i.MX Community - View the full discussion (https://community.freescale.com/message/336747#336747)

Sure, please follow this thread:

https://community.freescale.com/thread/306944

Reply to this message by replying to this email -or- go to the message on Freescale Community (https://community.freescale.com/message/336747#336747)

Start a new discussion in i.MX Community by email (mailto:discussions-community-imx@freescale-phx.hosted.jivesoftware.com ) or at Freescale Community (https://community.freescale.com/choose-container.jspa?contentType=1&containerType=14&container=2004)

>

0 件の賞賛
返信
1,829件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

yes.

First time I replied I pasted the wrong URL. Then I did edit my reply. I think you was not notified via email. Please see this:

https://community.freescale.com/thread/306901

0 件の賞賛
返信