compile for i.mx6d

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

compile for i.mx6d

Jump to solution
3,805 Views
niklasmolin
Senior Contributor I

Hi.

I have a project for the Sabresd board (Yocto).

What do I need to change to compile this project for an I.mx6d (dual)?

Thanks,

Niklas

Labels (2)
0 Kudos
Reply
1 Solution
3,553 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Niklas

     We normally use one kernel image for all i.MX6 SOCs. But for uboot, each board has each config, but for i.mx6d, it should be OK to use i.mx6q's config.

View solution in original post

0 Kudos
Reply
8 Replies
3,553 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, niklas

   Which kernel version you are using? As far as I know, for L3.10.17, no need to change anything for compiling i.mx6d, all i.MX6 platforms use same config.

0 Kudos
Reply
3,553 Views
niklasmolin
Senior Contributor I

Hi Yongcai.

I'm using Dora 1.5, so I think it is kernel 3.10.

So there is no difference in the compilation for the uBoot either then?

Thanks,

Niklas

0 Kudos
Reply
3,554 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Niklas

     We normally use one kernel image for all i.MX6 SOCs. But for uboot, each board has each config, but for i.mx6d, it should be OK to use i.mx6q's config.

0 Kudos
Reply
3,553 Views
niklasmolin
Senior Contributor I

Hi Yongcai.

I just wanted verify that I don't need to do any modification in the Linux image when running with an i.MX6D (I'm basing my image on SabdeSD).

I know that the SabdreSD has some CPU controlled voltage regulator, which we don't have in our design (plus we are using i.MX6D).

Right now I can get the kernel to boot on a SabreSD board, but in our custom board it hangs after "Starting kernel ...." after u-boot.

Just wanted to make sure that I don't need to change anything to run on an i.MX6D.

If the regulator is not setup, would that cause this kind of problem or would I see some print out from the kernel bootup?

Thanks,

Niklas

0 Kudos
Reply
3,550 Views
AnsonHuang
NXP Employee
NXP Employee

No, all ARM cores share a regulator, if regulator has problem, then your uboot will not be able to boot.

I think the problem is not caused by core number, but the difference of board design. You can add “nosmp” to uboot cmdline, then kernel will only boot up with one core.

Best Regards.

Anson Huang

Freescale Semiconductor Shanghai

Tel:021-28937058

0 Kudos
Reply
3,550 Views
niklasmolin
Senior Contributor I

Yongcai.

Before the Linux kernel is started, will the .dtb be applied?

If so, can there be any problem there, I have missed to change something the .dts/dtsi, so it causes the processor to stop?

Since the designed (how the power is provided) between the SabreSD and our custom board is different?

Best regards,

Niklas

0 Kudos
Reply
3,550 Views
AnsonHuang
NXP Employee
NXP Employee

Hi, Niklas

     dtb will be loaded to memory before kernel is started, for your case, I think you may need to enable early printk to see whether we can see any log when failed. After enable early printk in menuconfig, you need to add "earlyprintk" in cmdline to enable it.

3,550 Views
niklasmolin
Senior Contributor I

Hi Yongcai.

I managed to get it up and running.

Seems like there were too much ripple on our power to the ARM, so then we got an intermittent hanging of the processor.

Thanks,

Niklas

0 Kudos
Reply