compile for i.mx6d

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

compile for i.mx6d

跳至解决方案
5,811 次查看
niklasmolin
Senior Contributor I

Hi.

I have a project for the Sabresd board (Yocto).

What do I need to change to compile this project for an I.mx6d (dual)?

Thanks,

Niklas

标签 (2)
0 项奖励
回复
1 解答
5,559 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, Niklas

     We normally use one kernel image for all i.MX6 SOCs. But for uboot, each board has each config, but for i.mx6d, it should be OK to use i.mx6q's config.

在原帖中查看解决方案

0 项奖励
回复
8 回复数
5,559 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, niklas

   Which kernel version you are using? As far as I know, for L3.10.17, no need to change anything for compiling i.mx6d, all i.MX6 platforms use same config.

0 项奖励
回复
5,559 次查看
niklasmolin
Senior Contributor I

Hi Yongcai.

I'm using Dora 1.5, so I think it is kernel 3.10.

So there is no difference in the compilation for the uBoot either then?

Thanks,

Niklas

0 项奖励
回复
5,560 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, Niklas

     We normally use one kernel image for all i.MX6 SOCs. But for uboot, each board has each config, but for i.mx6d, it should be OK to use i.mx6q's config.

0 项奖励
回复
5,559 次查看
niklasmolin
Senior Contributor I

Hi Yongcai.

I just wanted verify that I don't need to do any modification in the Linux image when running with an i.MX6D (I'm basing my image on SabdeSD).

I know that the SabdreSD has some CPU controlled voltage regulator, which we don't have in our design (plus we are using i.MX6D).

Right now I can get the kernel to boot on a SabreSD board, but in our custom board it hangs after "Starting kernel ...." after u-boot.

Just wanted to make sure that I don't need to change anything to run on an i.MX6D.

If the regulator is not setup, would that cause this kind of problem or would I see some print out from the kernel bootup?

Thanks,

Niklas

0 项奖励
回复
5,556 次查看
AnsonHuang
NXP Employee
NXP Employee

No, all ARM cores share a regulator, if regulator has problem, then your uboot will not be able to boot.

I think the problem is not caused by core number, but the difference of board design. You can add “nosmp” to uboot cmdline, then kernel will only boot up with one core.

Best Regards.

Anson Huang

Freescale Semiconductor Shanghai

Tel:021-28937058

0 项奖励
回复
5,556 次查看
niklasmolin
Senior Contributor I

Yongcai.

Before the Linux kernel is started, will the .dtb be applied?

If so, can there be any problem there, I have missed to change something the .dts/dtsi, so it causes the processor to stop?

Since the designed (how the power is provided) between the SabreSD and our custom board is different?

Best regards,

Niklas

0 项奖励
回复
5,556 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, Niklas

     dtb will be loaded to memory before kernel is started, for your case, I think you may need to enable early printk to see whether we can see any log when failed. After enable early printk in menuconfig, you need to add "earlyprintk" in cmdline to enable it.

5,556 次查看
niklasmolin
Senior Contributor I

Hi Yongcai.

I managed to get it up and running.

Seems like there were too much ripple on our power to the ARM, so then we got an intermittent hanging of the processor.

Thanks,

Niklas

0 项奖励
回复