cfimager command for i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cfimager command for i.MX6

Jump to solution
12,328 Views
scott10
Contributor II

Hello Freescale Community,

I am trying to use Freescale's cfimager utility to quickly burn U-Boot images to an SD card at offset 0x400. I am able to burn the U-Boot image through Linux; however, I am looking for a Windows application to do this and cfimager seems like it should be capable of doing this for the i.MX6.

More specifically, I am looking for a way to burn the image u-Boot.imx to the SD card and have a FAT partition on top of U-Boot so I can copy other files to the card using Windows. I've done this using Linux, but I am curious whether cfimager can do this for me in a more convenient fashion. I've been able to use the following command to get cfimager to successfully burn u-boot.imx to the card and have it boot on my board:

cfimager -raw  -offset 0x400 –f u-boot.imx –d E   [where E is my drive letter]

Does anyone know if there is a way to have this file reside on the same SD card as a FAT filesystem? The cfimager documentation doesn't list anything about the i.MX6 or how to use the utility for that processor. I am using cfimager 1.7.2.001.

Thank you for your time.

Scott

Labels (4)
Tags (1)
0 Kudos
Reply
1 Solution
8,388 Views
Yuri
NXP Employee
NXP Employee

  Please use cfimager-imx as following :


cfimager-imx -a -offset 0x400 –f u-boot.imx –d E

(option -a is applied to format device always)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
10 Replies
8,389 Views
Yuri
NXP Employee
NXP Employee

  Please use cfimager-imx as following :


cfimager-imx -a -offset 0x400 –f u-boot.imx –d E

(option -a is applied to format device always)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
8,388 Views
scott10
Contributor II

Hi Yuri,

Thank you for the quick response!

I believe cfimager-imx is a different utility than the cfimager I was using. I was able to obtain a copy of cfimager-imx 1.2 copyright 2005 SigmaTel. I tried executing the command you listed above and it returned an error code: error -37.

Do you know what might be causing this error? Perhaps I have an obsolete version of cfimager-imx?

I saw another post with this error code in this forum, but I didn't see any resolution for the error code itself within the conversation: cfimager-imx can't download .bin file to SD

Here is a screenshot of my output:

cfimager-imx error 37.jpg

UPDATE:

I've been trying different things and if I use a 32GB SD card (instead of the 2GB card I was using) formatted as FAT32, I can use the cfimager application and the following command to achieve my result:

cfimager –raw –offset 0x400 –f u-boot.imx –d E –n

This allows me to put U-Boot at offset 0x400 and preserve the FAT32 filesystem so I can put additional files on the card using Windows.

I would still be curious to know what the "error -37" code means and whether there is a better way to do this. It would be helpful if I need to format a card and burn the image to the SD card using one command.

Thank you,

Scott

0 Kudos
Reply
8,388 Views
Yuri
NXP Employee
NXP Employee

I meant the cfimafer-imx for i.MX6. It may be found in Platform SDK

imx6_platform_sdk_v1.1.0.tar\iMX6_Platform_SDK\tools\windows\cfimager-imx.exe

https://www.freescale.com/webapp/Download?colCode=i.MX6_PLATFORM_SDK&location=null&fasp=1&WT_TYPE=So...

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
8,388 Views
scott10
Contributor II

Hi Yuri,

I downloaded the cfimager-imx utility from the link you provided and placed it in a folder containing u-boot.imx. When I try to execute the command you provided, I get error -34.

cfimager-imx error -34.jpg

I know the SD card works because I am able to use the method stated in my previous comment using cfimager (not cfimager-imx) to burn the image to the SD card. This allows me to boot U-Boot on my target system.

I've been experimenting with different commands for the cfimager-imx utility and I can never get it to format the SD card and write to it. Do we know what error codes -34 and -37 mean? More importantly, do we know how to fix this issue?

I can always fall back to the method stated in my previous comment to achieve my desired result, but finding a solution to this issue would not only help me, but it may help others in the future too.

Thank you,

Scott

0 Kudos
Reply
8,388 Views
Yuri
NXP Employee
NXP Employee

Please try to clear the SD using Linux command  dd, as shown below (an example)

$ sudo dd if=/dev/zero of=/dev/sda bs=512 count=1000

As for errors :

STERR_FAILED_TO_WRITE_SECTOR                                =     -37

STERR_UNABLE_TO_CALCULATE_CHS                               =     -34

~Yuri.

8,388 Views
scott10
Contributor II

Thank you Yuri. The cfimager-imx application works after writing the zeroes to the card.

Scott

0 Kudos
Reply
8,388 Views
blisslights
Contributor I

Scott, Yuri,

Can you guys help me with the command that can be used for CE.

We are using the following right now.

cfimager –f C:\CFIMAGER\nk.nb0 –d <sd card reader drive letter without colon> -imx53 –a

when it finishes issue the next command

cfimager –f C:\CFIMAGER\eboot.nb0 –d <sd card reader drive letter without colon> -imx53

So what will be the command for the above ce

cfimager –raw –offset 0x400 –f u-boot.imx –d E –n

will it be

cfimager –raw –offset 0x400  –f C:\CFIMAGER\nk.nb0 –d <sd card reader drive letter without colon> -imx53 –a –n

Thanks for your help.

0 Kudos
Reply
8,388 Views
Yuri
NXP Employee
NXP Employee

I have some doubts regarding cfimager parameter "offset". Usually nk.nb0

image does not require it, assuming nk.nb0 includes eboot image too and

should be written from  the beginning of SD card.

Regards,

Yuri.

0 Kudos
Reply
8,388 Views
blisslights
Contributor I

Thanks Yuri, 

Our problem is : using cfimager we are able to write to SD ( upto 2 GBs) but we are not able to write it to SDHC cards (having 8 GB or 32 GB) memory cards, do we need to specify something differently for SDHC cards, and what is it?

Again thanks for your help.

0 Kudos
Reply
8,388 Views
Yuri
NXP Employee
NXP Employee

As I remeber WinCE  in itself supports the SD High Capacity, but OEM  (Freescale, for example,
or Adeneo for i.MX6) should also provide it in SD driver.

If such SD driver can work with High Capacity it is specially mentioned in

corresponding WinCE release notes.

Please look at section SD MMC and Windows CE of the next for more details.

http://guruce.com/blogs/erwin

Regards,

Yuri.

0 Kudos
Reply