can not open include file 'gitversion.h'

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

can not open include file 'gitversion.h'

3,088 Views
LiuHui
Contributor I

I just follow the <Build Requirements.docx> in mfgtools\Apps\MfgTool.exe\docs to build the MFTTools sourcecode and finally it output an error message showing "Error 1 fatal error RC1015: cannot open include file 'gitversion.h'

 

Where can I get the 'gitversion.h' file?

thanks

0 Kudos
Reply
1 Reply

2,619 Views
ChrisWilliamson
Contributor III

Here's one. We have fixed the source extract script to generate this file when we do a source release so future versions will have this file. It is only used in the verioning of the MfgTool for our releases. You can feel free to change it however you see fit.

 

Chris

0 Kudos
Reply