bitbake fsl-image-validation-imx error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bitbake fsl-image-validation-imx error

Jump to solution
2,153 Views
Judy_Liao
Contributor II

Hi,

I set the build environment as following:

$ DISTRO=fsl-imx-wayland MACHINE=imx8mn-lpddr4-evk source imx-setup-release.sh -b build-8mnlpddr4-fslwayland

$ bitbake fsl-image-validation-imx

I got the errors:

ERROR: keyctl-caam-git-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'git://source.codeaurora.org/external/imx/keyctl_caam.git;protocol=https;branch=master')
ERROR: Logfile of failure stored in: /home/judy/bin/imx-yocto-bsp/build-8mnlpddr4-fslwayland/tmp/work/armv8a-poky-linux/keyctl-caam/git-r0/temp/log.do_fetch.31152
ERROR: Task (/home/judy/bin/imx-yocto-bsp/sources/meta-imx/meta-bsp/recipes-security/smw/keyctl-caam_git.bb:do_fetch) failed with exit code '1'

I check the error in the community, it seems  the error like this:

SRC_URI = "git://${PKG_NAME}.git;branch=main;protocol=https" 

 Initially it was 

 SRC_URI = "git://${PKG_NAME}.git;branch=master;protocol=https"

But, I just use $ bitbake fsl-image-validation-imx, how to fix the error?

Best regards,

Judy Liao

0 Kudos
Reply
1 Solution
2,127 Views
Judy_Liao
Contributor II

Thank you. I will try

View solution in original post

0 Kudos
Reply
2 Replies
2,142 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @Judy_Liao 

To git repository, It is now required to add a branch name as master.

Please check if you can access and download git://source.codeaurora.org/external/imx/keyctl_caam.git by manual on your build host, by which you can test the source provided by this link with git repository blocked or not in your network environment.

 

Best regards

Harvey

0 Kudos
Reply
2,128 Views
Judy_Liao
Contributor II

Thank you. I will try

0 Kudos
Reply