android 4.4.2 wifi softap mode!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

android 4.4.2 wifi softap mode!

10,353 次查看
liyu1
Contributor III

Hi all :

       Os : android 4.4.2

       Hardware imx6q , wifi module :rtl8188

      My Custom board Wifi function is ok ! But softap is not .  The log :

E/hostapd ( 4056): Configuration file: /data/misc/wifi/hostapd.conf

I/hostapd ( 4056): rfkill: Cannot open RFKILL control device

E/hostapd ( 4056): nl80211: Failed to set interface wlan0 into AP mode

D/CommandListener( 2266): Setting iface cfg

D/CommandListener( 2266): Trying to bring up wlan0

D/Tethering( 2644): Tethering wlan0

E/Tethering( 2644): Tried to Tether an unknown iface :wlan0, ignoring

E/WifiStateMachine( 2644): Error tethering on wlan0

E/hostapd ( 4056): nl80211 driver initialization failed.

E/hostapd ( 4056): Failed to initialize interface

W/audio_hw_primary( 2271): do_out_standby... 1107535256

   

How to solve this problem ?

标签 (2)
4 回复数

2,047 次查看
wilsonchen
Contributor III

HI,Li:

Can you share the way ?

0 项奖励
回复

2,047 次查看
jimmychan
NXP TechSupport
NXP TechSupport

You may read this for reference : http://www.daveconroy.com/turn-your-raspberry-pi-into-a-wifi-hotspot-with-edimax-nano-usb-ew-7811un-...

the hostapd that may not compatible with the rtl8188 chipset you used. So you may try to download the realtek driver and then compile it again to make the new hostapd.

hope this can help.

0 项奖励
回复

2,047 次查看
liyu1
Contributor III

Hi :

     I have resolved this issue ! Thanks ! 

2,047 次查看
wilsonchen
Contributor III

HI:

    Can you tell me the way that how to solve the problem ,I also met the same problem.This problem has troubled me for a long time.

thank you!!!

0 项奖励
回复