android 4.4.2 wifi softap mode!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

android 4.4.2 wifi softap mode!

10,486件の閲覧回数
liyu1
Contributor III

Hi all :

       Os : android 4.4.2

       Hardware imx6q , wifi module :rtl8188

      My Custom board Wifi function is ok ! But softap is not .  The log :

E/hostapd ( 4056): Configuration file: /data/misc/wifi/hostapd.conf

I/hostapd ( 4056): rfkill: Cannot open RFKILL control device

E/hostapd ( 4056): nl80211: Failed to set interface wlan0 into AP mode

D/CommandListener( 2266): Setting iface cfg

D/CommandListener( 2266): Trying to bring up wlan0

D/Tethering( 2644): Tethering wlan0

E/Tethering( 2644): Tried to Tether an unknown iface :wlan0, ignoring

E/WifiStateMachine( 2644): Error tethering on wlan0

E/hostapd ( 4056): nl80211 driver initialization failed.

E/hostapd ( 4056): Failed to initialize interface

W/audio_hw_primary( 2271): do_out_standby... 1107535256

   

How to solve this problem ?

ラベル(2)
4 返答(返信)

2,180件の閲覧回数
wilsonchen
Contributor III

HI,Li:

Can you share the way ?

0 件の賞賛
返信

2,180件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

You may read this for reference : http://www.daveconroy.com/turn-your-raspberry-pi-into-a-wifi-hotspot-with-edimax-nano-usb-ew-7811un-...

the hostapd that may not compatible with the rtl8188 chipset you used. So you may try to download the realtek driver and then compile it again to make the new hostapd.

hope this can help.

0 件の賞賛
返信

2,180件の閲覧回数
liyu1
Contributor III

Hi :

     I have resolved this issue ! Thanks ! 

2,180件の閲覧回数
wilsonchen
Contributor III

HI:

    Can you tell me the way that how to solve the problem ,I also met the same problem.This problem has troubled me for a long time.

thank you!!!

0 件の賞賛
返信