an error was encountered while installing and opening project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

an error was encountered while installing and opening project

730件の閲覧回数
melanie
Contributor III

Hi 

Q1:I already have version 11.6 installed, can I install version 11.7 without deleting version 11.6?

install version11.7 when version11.6 is here

melanie_0-1691375946940.pngmelanie_1-1691376081714.png

Q2:my project is bulid by version11.7 .   could I use version 11.6 open it successfully?

0 件の賞賛
返信
1 返信

693件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi @melanie 

To Q1, I tried to reproduce, but no such issue as yours.

To Q2, In principle, it is not recommended to use it from the perspective of IDE, and the new options on the higher version may be lost in the lower version.

 

Best regards

Harvey

0 件の賞賛
返信