i.mx6ull usb audio class 2.0 driver problem on linux-4.1.15

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.mx6ull usb audio class 2.0 driver problem on linux-4.1.15

899件の閲覧回数
frank0529
Contributor I

Hello there,

https://community.nxp.com/t5/i-MX-Processors/Can-iMX7ULP-or-iMX8-act-as-USB-Audio-Class-2-0-device/t...

according to the link above, I apply the patch on linux-4.19.35 to fix the yellow mark in Win10 Device Manager and successfully drive i.mx6ull as a usb soundcard, both capture and playback are OK. But I do the same thing on linux-4.1.15,  executing aplay on i.mx6ull is working well, but executing arecord will report error:

arecord: pcm_read:2096: read error: Input/output error.

seems no audio data is captured, I'm not sure which part I'm missing.

I couldn't use linux-4.19.35 directlly because the kernel will be stuck when I access to some memory area, such as execute readl or insmod kernel module, it seems some memory area is protected by certain function, I disable the OPTEE and the problem is still exist.

hope someone can help me, thanks a lot.

ラベル(1)
0 件の賞賛
返信
1 返信

880件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Please check the capture (input) is enable or not in the alsamixer.

0 件の賞賛
返信