an error was encountered while installing and opening project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

an error was encountered while installing and opening project

1,196 次查看
melanie
Contributor III

Hi 

Q1:I already have version 11.6 installed, can I install version 11.7 without deleting version 11.6?

install version11.7 when version11.6 is here

melanie_0-1691375946940.pngmelanie_1-1691376081714.png

Q2:my project is bulid by version11.7 .   could I use version 11.6 open it successfully?

0 项奖励
回复
1 回复

1,159 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @melanie 

To Q1, I tried to reproduce, but no such issue as yours.

To Q2, In principle, it is not recommended to use it from the perspective of IDE, and the new options on the higher version may be lost in the lower version.

 

Best regards

Harvey

0 项奖励
回复