about EMMC Memory driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about EMMC Memory driver

1,492件の閲覧回数
俊宝胡
Contributor I

I want change  EMMC  chip, What do I need to change the kernel and uboot.

I used  i.MX 6Quad

Linux BSP Source Code: L3.0.35_4.1.0_ER_SOURCE_BSP

Thanks

ラベル(1)
0 件の賞賛
返信
1 返信

1,386件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 俊宝 胡

eMMC is standard device and all supported eMMC should work fine.

So no need to change uboot/linux sources.

However for boot one may have to set correct boot settings,

this is described in Chapter System Boot  i.MX6 Reference Manual.

sect.8.5.3 Expansion Device IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信