imx6dl boot source

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6dl boot source

1,675 次查看
arkadiuszkaras
Contributor I

Hello,

With imx6, is there any possibility to check from which interface ROM loaded boot stream ?

I need to know in u-boot from which device it was loaded.

Regards

AK

标记 (2)
0 项奖励
回复
1 回复

1,556 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Arkadiusz

yes, this could be done using

SRC Boot Mode Register 1 (SRC_SBMR1,2)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复