Issues About i.Mx6SL LPDDR2 Script Aid configuration options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues About i.Mx6SL LPDDR2 Script Aid configuration options

1,294 Views
tony_l_cai
Contributor III

Hi,All

       in i.Mx6SL LPDDR2 Script Aid ,some  configuration options is confused. Because my LPDDR2  total density is 512Mb, DRAM single die density (Gb)DRAM density(Gb)DRAM density per CS (Gb) , how to fill in these blanks? 3Q~

Labels (2)
0 Kudos
Reply
1 Reply

1,150 Views
igorpadykov
NXP Employee
NXP Employee

Hi tony

one can look at example below

Example.jpg

and other lpddr2 init examples in SDK

i.MX 6Series Platform SDK : Bare-metal SDK

Interleaved LPDDR2 Memory on i.MX6Dual

i.Mx6DQSDL LPDDR2 Script Aid

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------