about EMMC Memory driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

about EMMC Memory driver

967 Views
俊宝胡
Contributor I

I want change  EMMC  chip, What do I need to change the kernel and uboot.

I used  i.MX 6Quad

Linux BSP Source Code: L3.0.35_4.1.0_ER_SOURCE_BSP

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

861 Views
igorpadykov
NXP Employee
NXP Employee

Hi 俊宝 胡

eMMC is standard device and all supported eMMC should work fine.

So no need to change uboot/linux sources.

However for boot one may have to set correct boot settings,

this is described in Chapter System Boot  i.MX6 Reference Manual.

sect.8.5.3 Expansion Device IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply