Yocto build error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto build error

3,502件の閲覧回数
erikraynolds
Contributor IV

Dears,

I'm getting error by Yocto build when local.conf adds:

IMAGE_INSTALL_append += " vim"

by building it:

Build Configuration:
BB_VERSION = "1.26.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Debian-8.2"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qpsabreauto"
DISTRO = "fsl-imx-x11"
DISTRO_VERSION = "3.14.52-1.1.1"
TUNE_FEATURES = "arm armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU = "vfp-neon"
meta
meta-yocto = "(nobranch):b74ea963cefffad9fbd91d4eb9b240f6a8c86cd0"
meta-oe
meta-multimedia = "(nobranch):df2f700d66bace65f5d802225232d01cf511fe81"
meta-fsl-arm = "(nobranch):70ddee3ebeacbc53180ee7221533375bf0c9eac4"
meta-fsl-arm-extra = "(nobranch):41e79c6bd055f12b6252618c22c43a2fed5cfb49"
meta-fsl-demos = "(nobranch):17f9da65efb5c65c1d44b5cc18584034b29a742b"
meta-bsp
meta-sdk = "(nobranch):46b952b39b012cadc8a91b551ed3beee16054768"
meta-browser = "(nobranch):30b8d6b3d0d6501c56ef6967a2fa73a3d4bf5fe9"
meta-gnome
meta-networking
meta-python
meta-ruby
meta-filesystems = "(nobranch):df2f700d66bace65f5d802225232d01cf511fe81"
meta-qt5 = "(nobranch):51b4620392aa9041d8512549bfa554bea368c5ea"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: No checksum specified for /mnt/work/Linux/PeterB/fsl-release-3.14.52-1.1.0_ga/downloads/vim_vim.googlecode.com_.hg._v7-4-481.tar.gz, please add at least one to the recipe:
SRC_URI[md5sum] = "f3c7295c7e542fba141c2f3d0ac8765c"
SRC_URI[sha256sum] = "0f5419388b70c62154ff3d027396b09e5acc0f028cb0ba9ce73f242d02613c39"
ERROR: Function failed: Fetcher failure for URL: 'http://downloads.yoctoproject.org/mirror/sources/vim_vim.googlecode.com_.hg._v7-4-481.tar.gz;protoco...'. Missing SRC_URI checksum
ERROR: Logfile of failure stored in: /work/Linux/fsl-release-3.14.52-1.1.0_ga/build-x11-full/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/vim/7.4.481-r0/temp/log.do_fetch.19256
ERROR: Task 574 (/work/fsl-release-3.14.52-1.1.0_ga/sources/meta-openembedded/meta-oe/recipes-support/vim/vim_7.4.481.bb, do_fetch) failed with exit code '1'

タグ(1)
0 件の賞賛
返信
1 返信

2,774件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Erik Raynolds,

It seems that this recipe, which is part of Open Embedded, is broken and the repository where the source was it-s no longer there.

It looks like the following bug:

https://www.yoctoproject.org/bug/bug-8253-vim-recipe-broken

The problem is that the BSP Release you are using refers to a specific commit in the past unlike the Community BSP which is constantly changing. My recommendation would be switching to the 4.1.15 BSP Release to see if the recipe is fixed there.

Another alternative would be looking for the new repository for this recipe and manually fixing it.

https://layers.openembedded.org/layerindex/recipe/5559/

I hope this information helps!

Regards,

0 件の賞賛
返信