Yocto Build Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto Build Error

3,130件の閲覧回数
engineer_bsp01
Contributor III

Hi,

I'm trying to get familiar with yocto project for imx6qsabreauto.I'm referring imx_yocto_userguide.I get following error every time executing the command 'bitbake core-image-base'.

ERROR: Unable to start bitbake server
ERROR: Last 10 lines of server log for this session (/home/BspDeveloper2/fsl-community-bsp/build/bitbake-cookerdaemon.log):
Traceback (most recent call last):
  File "/home/BspDeveloper2/fsl-community-bsp/sources/poky/bitbake/lib/bb/daemonize.py", line 77, in createDaemon
    function()
  File "/home/BspDeveloper2/fsl-community-bsp/sources/poky/bitbake/lib/bb/server/process.py", line 433, in _startServer
    self.cooker = bb.cooker.BBCooker(self.configuration, self.featureset)
  File "/home/BspDeveloper2/fsl-community-bsp/sources/poky/bitbake/lib/bb/cooker.py", line 178, in __init__
    self.configwatcher = pyinotify.WatchManager()
  File "/home/BspDeveloper2/fsl-community-bsp/sources/poky/bitbake/lib/pyinotify.py", line 1764, in __init__
    raise OSError(err % self._inotify_wrapper.str_errno())
OSError: Cannot initialize new instance of inotify, Errno=Too many open files (EMFILE)

 

I have no idea about this.

Please help me to sort out the same..

Regards,

Richu C J

0 件の賞賛
返信
1 返信

2,620件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Which BSP are you using?

Is it work if you build core-image-minimal?

0 件の賞賛
返信