Writing bootloader failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Writing bootloader failed

Jump to solution
19,757 Views
AlekseyM
Contributor III

Hi! I make a custom board with iMX8MM and compile u-boot. But I can't understand what I do wrong. Could somebody tip me?
I use uuu under Windows 10, for compiling images I use imx-boot under WSL2 ubuntu 20.04.
Log by board:

 

MMC:   FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... MMC: no card present
*** Warning - No block device, using default environment

MMC: no card present
Detect USB boot. Will enter fastboot mode!
Net:   Could not get PHY for FEC0: addr 0
Could not get PHY for FEC0: addr 0
No ethernet found.

Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for                                mfgtools
, using default environment

Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot:  0

## Checking Image at 43800000 ...
Unknown image format!
Run fastboot ...
Detect USB boot. Will enter fastboot mode!
flash target is MMC:1
MMC: no card present
MMC card init failed!
MMC: no card present
** Block device MMC 1 not supported
Detect USB boot. Will enter fastboot mode!
flash target is MMC:2
switch to partitions #0, OK
mmc2(part 0) is current device
Detect USB boot. Will enter fastboot mode!
Starting download of 2091712 bytes
...............
downloading of 2091712 bytes finished
writing to partition 'bootloader'
Initializing 'bootloader'
switch to partitions #1, OK
mmc2(part 1) is current device
Writing 'bootloader'

MMC write: dev # 2, block # 66, count 4086 ... MMC: block number 0x1038 exceeds max(0x1000)
0 blocks written: ERROR
Writing 'bootloader' FAILED!

 

 Log by uuu

 

FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}
FB: flash bootloader flash.bin
FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;
FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: Done


Wait for Known USB Device Appear...
New USB Device Attached at 1:2
1:2>Start Cmd:SDP: boot -f flash.bin
100%1:2>Okay (0.452s)
New USB Device Attached at 1:2
1:2>Start Cmd:SDPV: delay 1000
1:2>Okay (1.013s)
1:2>Start Cmd:SDPV: write -f flash.bin -skipspl
100%1:2>Okay (2.913s)
1:2>Start Cmd:SDPV: jump
100%1:2>Okay (0.244s)
New USB Device Attached at 1:2
1:2>Start Cmd:FB: ucmd setenv fastboot_dev mmc
1:2>Okay (0.016s)
1:2>Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}
1:2>Okay (0.049s)
1:2>Start Cmd:FB: ucmd mmc dev ${emmc_dev}
1:2>Okay (0.054s)
1:2>Start Cmd:FB: flash bootloader flash.bin
0x40000000Write partition failed1:2>Fail Write partition failed(0.13s)

 

0 Kudos
Reply
1 Solution
19,540 Views
smithcoba
Contributor III

Here is your log.

Detect USB boot. Will enter fastboot mode!
Starting download of 2091712 bytes
...............
downloading of 2091712 bytes finished


MMC write: dev # 2, block # 66, count 4086 ... MMC: block number 0x1038 exceeds max(0x1000)

The space you must have on boot1: 

66 x 512 +  2091712  = 2,125,504

The space on the emmc boot1:

4096 x 512 = 2,097,152

2,097,152 -  2,125,504  =  -28,352

The emmc is 32G, it is user partition. not boot partition. 

The log shows the boot partition is 2M big. That I have told you before.

If you use scard, the flash.bin can flash into it. 

 

Usually, the NXP binary demo image flash.bin is bigger than 2M.

If you want use the emmc currently on your board, you must change the uboot configuration to make it smaller.

 

 

image.png

View solution in original post

23 Replies
2,443 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @AlekseyM !

For your custom board, you have to create our custom DDR training based on your custom board.

Please follow the attached guide to update the ddr training and ddr timing on your board.

 

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Family-DDR-Tool-Release/ta-p/110...

 

0 Kudos
Reply
2,409 Views
AlekseyM
Contributor III

Yes, of course, I created timing.c from DDR-tool. Without this my ddr4 not initiate.

0 Kudos
Reply
2,571 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @AlekseyM!

 

Thank you for contacting NXP Support!

What command are you using under uuu?

If you want to download the bootloader to iMX8, you have to put the board in download mode and then use the next command:

./uuu.exe -b <boot_type> flash.bin

boot_type could be:

emmc

sd

fspi

I attached the UUU guide to understand better the commands that you can use for all iMX devices.

Best Regards!

Chavira

0 Kudos
Reply