I'm using iMX8MP EVK with Yocto Kirkstone (wayland) platform to drive two displays (HDMI+LVDS0). The wayland runs in extended desktop mode. Both display interfaces are working, the wayland toolbar is visible on both displays.
How can I auto launch an application programmatically on the secondary display? The apps launched from command line always are displayed on the first display.